Wi-Fi Combo Forum Discussions
I am looking to explore prototyping with the BCM2835, but am somewhat hampered by not having access to the BCM2835's BGA pinouts. If schematic symbols and packages exist with these pinouts already mapped, that would be wonderful.
Show LessDear,
I hope to get a sample source code for IIS interface working on WICED 2.4.1.
I want to test for audio.
If you have it tested, please let me get it.
Thank you all.
Gideon
Show LessWhenever I do a push or pop operation to a queue in SDK 3.0.1, the platform locks up. Any idea why this might be? My code is below:
static wiced_queue_t slave_queue;
wiced_rtos_init_queue (&slave_queue,NULL,10,10);
WPRINT_APP_INFO(("%d items\n",slave_queue.handle.tx_queue_enqueued));
WPRINT_APP_INFO(("Pushing\n"));
wiced_rtos_push_to_queue (&slave_queue, "oh hai ",200);
WPRINT_APP_INFO(("%d items\n",slave_queue.handle.tx_queue_enqueued));
Show LessOur requirement is that we need to write the certificate into the DCT security section.
We are using wiced_dct_write_security_section API, which is declared in wiced_dct.h header file. We are passing pointer to structure platform_dct_security_t to this API, which holds private key, certificate and cookey.
Now the problem is, this API is only writing certificate in DCT memory. When looking at the code of this API, it takes argument data pointer and simply writes it down into the certificate section of DCT, instead of first taking offset up to certificate data in provided argument. Because of this it will always write Private key of the provided argument into DCT certificate memory. Snippet here:
config.c file line 121:
wiced_result_t wiced_dct_write_security_section( const platform_dct_security_t* security_dct )
{
int result = bootloader_api->write_certificate_dct( 0, (void*)security_dct, sizeof( *security_dct ) );
return ( result == 0 ) ? WICED_SUCCESS : WICED_ERROR;
}
bootloader.c file line 210:
static int write_certificate_dct( unsigned long data_start_offset, void* data_in_addr, unsigned long num_bytes_to_write )
{
return platform_write_dct( OFFSET(platform_dct_data_t, security_credentials) + OFFSET(platform_dct_security_t, certificate)- sizeof(platform_dct_header_t) + data_start_offset, data_in_addr, num_bytes_to_write, -1, NULL );
}
Hello,
We are using Wiced SDK 2.4.0 for SN8200 platform. We are looking for packet broadcasting support in TCP or UDP.
Is Packet broadcasting support available for TCP or UDP in wiced sdk?
If yes, where we can find its API guide and Sample application?
Is there mesh network support available in wiced SDK?
Any help in this case is appreciated.
Waiting for your reply.
Thanks,
Nipam
Show LessHi,
I found issues (lead to often tcp connect failure in wiced_http_get) if i'm trying to call wiced_http_get on more than one threads... From the look of wiced_http_get it seems Thread safe but i cannot be 100% sure. This issue can only be reproduced if i leave it running for hours with 2 thread calling wiced_http_get with 1 seconds delay after operation return (either success or failure). Does anyone has any idea?
Best Regards,
Aaron Lee
Show LessHi,
When I test the OTA function, I get a fail sometimes.
After success message of upgrade, our board run a application in SFLASH.
Now, I am using SST25VF080B.
If you have any idea or suggestion, let me know it please.
Thank you.
Gideon.
Show Less