Wi-Fi Combo Forum Discussions
Hi,
This is to report WPS issues on LwIP.
Testing on 3.0.1 SDK.
Build with "test.console-FreeRTOS-LwIP-BCM943362WCD4 download run", then
WPS test looks OK.
Build with "test.console-FreeRTOS-LwIP-BCM943362WCD4 download run", then
WPS PBC and PIN modes test always fails.
Below shows the log:
> join_wps pin 12345670
Starting Enrollee in PIN mode
> Starting WPS Enrollee
Joining '��������������������������������������������������������������������������������������������������������������������������������������������'
Joining '��������������������������������������������������������������������������������������������������������������������������������������������'
Joining '��������������������������������������������������������������������������������������������������������������������������������������������'
Joining '��������������������������������������������������������������������������������������������������������������������������������������������'
Joining '��������������������������������������������������������������������������������������������������������������������������������������������'
( Just endless Joining '..... )
Show Lessp2p :
void application_start( )
{
wiced_init();
besl_p2p_init ( &workspace, &device_details );
besl_p2p_start( &workspace );
}
but I don't know how to communication with Android mobile phone?
Show LessMy customer has some installations where they can not deploy wireless or need to to be shutdown. In this case we want to use the same design and add an optional Ethernet controller for wired connectivity. The speed could be 10Mbps
Thanks
Show LessIf you call "netif_set_down" followed by "netif_remove" followed by "wiced_wifi_leave" on an Aruba network during a shaky connection after wiced posts the LINK_LOST event, wiced will no longer be able to negotiate DHCP with the network through Aruba APs regardless of the make/model of the network controller. The Aruba APs seem to receive the packet and just ignore it never passing it on to the Controller/DHCP server.
Show LessWhat is the replacement/equivalent of the functions wiced_dct_read_wifi_config_section and wiced_dct_write_wifi_config_section in sdk 3.0.1? These functions are listed as depreciated in the API.
Show LessHello,
I discover that OTA upgrades are unavailable in Wiced 3.0: core functions (platform_load_ota_app ...) emptied and apps/waf/ota_upgrade sample app removed!
Will such an important feature be available back soon ?
Furthermore, we would like to implement OTA in a different way, a bit like how apps/waf/sflash_write does: The new firmware would be downloaded and written to the SPI flash, then the boot-loader would copy it to internal MCU flash at next reboot (not at the end of download).
I've been looking at the sflash_write app code but I can't figure out how it works because it is driven by an external TCL script ( openOCD). Any help would be appreciated.
Best regards,
Pascal.
Show LessAre there any intentions or demo projects to use WICED Smart (BLE) with modern Mobile App Development Platforms?
I would like to use one of the following IDEs:
Nokia Qt - expected version 5.4 should have BLE support
Embacadero RADStudio XE7 - works already for me on a BLE devices
Xamarin - looks promising (especially for remote iOS build in parallel with Android)
The benefit: all major platforms could be supported by: "code just once and build for several targets and OS".
Please, could you think about to support such Development Platforms (IDE) as part of WICED SDK etc.?
(e.g. to have App demo projects not just as Android SDK, nice to have also for these IDEs)
BTW:
It would be great if WICED SDK could be part if such an IDE:
If I develop the FW for the WICED device, e.g. a BLE sensor - a seamless integration or reuse of files, e.g. XML based GATT
server definitions, so that the related App counterpart would be consistent or "generated in a half-automated" way.
Or v.v: from the App development the WICED SDK is fed with info to create counterpart FW skeleton, e.g. to use same GATT, XML files, to keep App and Device FW consistent.
Thank you.
Show LessHello
Whatever bloc size (1, 2, 4, 8Ko) I try to write to the spi flash (sflash_write), I get a constant very slow throughput: 13 seconds for each KiB written.
Having a look at spi_flash.c make me think that low level writes are done one byte at a time.
Any advice to increase write throughput would be appreciated.
Thanks in advance,
Pascal
Show LessSummary Issue or question:
I cannot build the example code
SDK version
2.4.1
HW Platform (if it is a peripheral or MCU issue)
Show Less**** Build of configuration Default for project Wiced-SDK ****
C:\Users\dcairns\Documents\WICED\WICED-SDK-2.4.1\Wiced-SDK\make.exe Default
Making config file for first time
wiced_config.mk:150: *** Unknown component: Default. Stop.
make: *** No rule to make target 'build/Default/config.mk', needed by 'main_app'. Stop.