Wi-Fi Combo Forum Discussions
I am trying to debug a simple program, testing PWM, but when I initiate the debugger get a message stating 'Launching WICED debug' has encountered a problem
Error in final launch sequence
The screen shot is attached.
I have reviewed the step by step setup for debugging and the settings appear to be the same. The target I am using is an: ISM43362_M3G_L44
I am able to build and download and run other apps.
Thanks in advance.
Show LessHi,
I try to run bt_smartbridge Demo Application on my BCM943341WCD1 EVB. I use SDK 3.1.1.
I connect successfully to the board´s Web page through a shared Wifi Access Point.
Then a ask for BT devices scanning pushing "Rescan" button.
The "Scanning for Bluetooth Smart devices ..." message appears.
But then I get "No device found". I get the same result repeating several time these steps.
And however there are many devices Bluetooth devices around the EVB.
Do you have some idea about what could be wrong in my test?
Thanks
Regards,
Julien
Show LessHi,
I would like to the second UART interface (UART2) of BCM943341WCD1 module.
But I see in platform.h that there is only one UART usable: UART1 reserved for STDIO traces.
Is it a platform limitation? or the code that would support UART2 is just missing and I need to add it?
I am using SDK 3.1.1
Thank you!
Regards
Julien
Show LessI am using WICED SDK 2.4.1 with USI BM-09 but I need to migrate to 3.1.1 SDK.
When do you include BCMWCDUSI09 platform to SDK?
I know, BCMWCDUSI09 module is BCM943362+STM32F02
Can BCM943362WCD4 be subsituted for BCMWCDUSI09?
Show LessHi,
I am using a WICED Wifi board. I have been trying to send data to the server through TCP socket every 2 seconds. I could get the connection between the server and board established and I was also able to sent data through the established socket. But after some random time, the sending function failed though the connection was still alive.
A more elaborate explanation of my problem is below.
I created the socket, binded it to a port and established the connection with the server. I created the packet using wiced_packet_create_tcp() and sent the data using wiced_tcp_send_packet() every 2 seconds. The server was able to receive the data. This went fine only for sometime. After that the wiced_tcp_send_packet() function fails each time. I took care of deleting packet using wiced_packet_delete().
Next, I used wiced_tcp_send_buffer() instead of wiced_tcp_send_packet(). Same problem.
I also used wiced_tcp_stream_init(), wiced_tcp_stream_write() and wiced_tcp_stream_flush() functions to send data, instead of the above functions. Still it's the same.
Is anything missing or there is some problem in WICED API of sending tcp packet.
Thanks
Show LessIs there support for the BCM43341 which is used on the Intel Edison. We have some problems to download on the Intel Edison the new firmware for the BCM43341. We tried this with a previous version and the system fails to end this download to the Intel Edison module (hang-up)
Show Less
Hi,
I'm planning to use SN8000 WiFi module and WICED SDK running in STM32 MCU. I want to interface SD card also over SPI? Is FAT file system support available with WICED SDK(with any of the RTOS)? Is there any solution already available for interfacing with SD card over SPI?
Best Regards,
Deepa.
Show LessNext question,
Which hardware I have to use to develop new software/firmware for this SoC (BCM 43341). I signed already the NDA
Best Regards,
Piet
Show LessI am looking at the implementation of wiced_spi_init and wiced_spi_deinit and they are the same in wiced_platform_common.c... Is this a bug or design feature? I would have expected wiced_spi_deinit to call platform_spi_deinit and I would also have expected platform_spi_deinit to at least return WICED_SUCCESS if it has no current work to do.
Show Less