Wi-Fi Combo Forum Discussions
As it said in title
hello
- What’s DCT in WICED? What’s it for? Is there already any doc in WICED Community?
- What’s the purpose of files DCT.elf/DCT.bin/DCT* ?
- How DCT is built? What source files are contained? What’s the build process?
- Find a way for assembly line to create different DCT for different device.
thanks!
Show LessI am considering using MQTT for communication between the controller and server because it is really light-weight and compatible for IoT. Does WICED support this protocol? If not, any future plans to support it?
Show LessHello,
Does WICED support 40 Mhz ? We use BCM9WCDUSI09.
When we upload mfg_test and try to set bw to 40 mhz by typing command "chanspec -c 1 -b 2 -w 40 -s 0", we observe the same occupied BW with chan bandwidth=20 ("chanspec -c 1 -b 2 -w 20 -s 0") on RF spectrum analyzer.
If it does 40 Mhz, what is the reason behind this situation?
Thanks,
Mert
Show LessIm running into an issue that i want to attribute to low memory but i have no way of profiling whether i have a memory leak.
Is there a runtime code analyzer running on the WICED platform that could be used to profile?
Thanks.
Show Less- Test case
1: Iperf TCP test, EVB as iperf server,
Wi-Fi station as iperf client.- Input command “iperf –s” to enable the iperf server
on EVB side.
- Input command “iperf –s” to enable the iperf server
i dont know that how to input the command "iperf -s",i do that show :
what can i do ?
Thanks!
Show LessHello,
The ota webpage didn't work properly in Internet Explorer 11, when clicking the "start upgrade" button it returned an invalid state error.
This can be fixed inside "ota_server_web_page.c" by moving:
" xhr.timeout = 2000;\r\n" \
to below
" xhr.open('POST', upgrade_chunk_url_with_query , true);\r\n" \
IE apparently doesn't allow to set the timeout before the connection is opened.
Cheers,
Gerard
Show LessI am using WICED SDK 3.1.2. I am able to use http_stream_t session and do a HTTP POST to webserver successfully. I want to do a HTTPS POST to webserver. Is there an equivalent to http_stream_t for HTTPS POST? Is there a sample code available that shows how to do a HTTPS POST using WICED SDK 3.1.2?
Thanks,
-janaki
Show LessWho have BCM943362wcd6 sch&layout?share me.