Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Wi-Fi Combo Forum Discussions

Anonymous
Wi-Fi Combo
I've tried to create two http server instances - one for the config interface followed by another http server for the STA interface.The STA interface'... Show More
Anonymous
Wi-Fi Combo
I am trying to hook up an SPI device but am confused about which SPI interface to use. I am using 3.1.2 SDK with the WCD4_EVB.The only one defined in ... Show More
Anonymous
Wi-Fi Combo
I have a TCP serve app in which two sockets are opened in two threads/tasks, and they are in blocking state which waits for some data.Socket 1 expects... Show More
Anonymous
Wi-Fi Combo
Hi,I am trying to bring up a WCD4_EVB on a Windows 8.1 machine. I have downloaded and installed the 3.1.2 WICED IDE but the drivers (apparently) did n... Show More
Anonymous
Wi-Fi Combo
This wiced_time_get_iso8601_time() does not do a bitwise AND of a number that is frequently greater than 65000, when it converts to a uint16_t. Conseq... Show More
Anonymous
Wi-Fi Combo
Hi,     Currently we are using SDK 3.1.2 version, In this we tried to execute snip.email with the  EVB BCM9WCDPLUS114. But we are facing the following... Show More
Anonymous
Wi-Fi Combo
Hi,I'm debugging a tcp transfer test that the receiver does not receive data correctly.Then I found wiced_tcp_send_buffer() may return 16 (WICED_WOULD... Show More
Anonymous
Wi-Fi Combo
Hello!I have problem when establish TCP connection in softAP mode, the wifi module running softAP and DHCP mode to asign IP to client,  I want wifi ac... Show More
Anonymous
Wi-Fi Combo
Greetings,I have installed the WICED SDK 2.40 on an XP 32bit machine. The program is installed properly. I have downloaded the MinGW GCC and set it as... Show More
Anonymous
Wi-Fi Combo
If I want  to  use WICED_UART_2, which pins on the ST micro would this map to?I'm using the ISM43362_M3G_L44 module. Show More
Forum Information

Wi-Fi Combo

Discussion forum regarding WICED Studio Wi-Fi Combo topics.