Wi-Fi Combo Forum Discussions
text.format{('custom.tabs.no.results')}
Hi,
I've looked a lot inside the forum about the OTA process but unsuccessfully, I did not found my answer...
I've wrote an application which load a tcp client located in FR_APP on a BCM943362WCD4_EVB.
This app located in FR_APP is receiving chunck of a file and writing it on the APP0 location.
When I received all chuncks, I reboot the wiced.
Initialization :
- wiced_framework_app_open
- wiced_framework_app_get_size
- wiced_framework_app_set_size
- wiced_framework_app_get_size
Chunck writing :
- wiced_framework_app_write_chunk
Rebooting :
- wiced_framework_app_close
- wiced_framework_set_boot
My problem is that, as I change the boot configuration, the module never reboot and I'm obliged to reflash it to work properly.
Moreover, I looked trough the internal flash, and nothing has been wrote at 0x0800C000
Any help would be appreciated,
Regards.
Show LessHi all!
I am using WICED-SDK 3.1.2 transplanted to our own platform (lwip + RTOS). SPI bus Interface.
In STA mode, when successfully joined an AP , I found BCM43362 can not receive broadcast packets(such as ARP packets), It seems like all broadcast packets were filtered out, and the BCM43362 did not trigger MCU GPIO Interrupt. However, other types of packets received properly, the TCP and UDP can be normal operation.
I used WLC_SET_PROMISC option enable promiscuous mode, it is still invalid.
Can anyone help me?
消息编辑者为:tao yang
Show LessIs there a plan to release a Mac pkg for WICED 3.3.1?
- Ajay
Hi,
I am using wiced wifi 3.3.1 sdk in which ble is in peripheral mode.
I have two questions related to ble advertisement
1] How to set advertisement flag as general to advertise indefinitely, currently advertises for 90 seconds, then stops advertising. I can see MACRO "BTM_BLE_GENERAL_DISCOVERABLE_FLAG" but can't see any API to set advertisement indefinitely(General).
2] How to set advertising data( manufacture data & list of supported services).
e.g. I need to set manufacture data as 1122334455 & add list of supported services i.e temperature service with UUID 0xFFF0.
Hi All,
I apologize if this is an obvious question, but can the WICED SDK be used for the BCM4343W single-band wifi + BLE chip? I know it is listed under "WICED Wi-Fi" on the website, but it doesn't come up in searches on the forum. E.g. can the BCM943362WCD6 EVB target be used to develop for the less-capable chip?
Thank you for your guidance.
Sincerely,
Steve
Show LessThere's a typographical makefile error in WICED-SDK/tools/makefiles/wiced_apps.mk that causes WICEDv3.1.2 to fail to build, but only in the event that APP2 is defined. The APP0_DOWNLOAD target gets defined twice assuming both APP0 and APP2 are defined. In the seccond instance should really be APP2_DOWNLOAD. See makefile excerpt below.
ifneq ($(APP0),)
APP0_DOWNLOAD: $(APP0_DOWNLOAD_DEPEDENCY)
$(QUIET)$(ECHO) Downloading APP0 ($(APP0)) at sector $(APP0_SECTOR_START)...
$(call CONV_SLASHES,$(OPENOCD_FULL_NAME)) -f $(OPENOCD_PATH)$(JTAG).cfg -f $(OPENOCD_PATH)$(HOST_OPENOCD).cfg -f apps/waf/sflash_write/sflash_write.tcl -c "sflash_write_file $(APP0) $(APP0_SECTOR_ADDRESS) $(SFLASH_APP_PLATFROM_BUS) 0 $(SFLASH_APP_BCM4390)" -c shutdown #$(DOWNLOAD_LOG) 2>&1
endif
ifneq ($(APP1),)
APP1_DOWNLOAD: $(APP1_DOWNLOAD_DEPEDENCY)
$(QUIET)$(ECHO) Downloading APP1 ($(APP1)) at sector $(APP1_SECTOR_START)...
$(call CONV_SLASHES,$(OPENOCD_FULL_NAME)) -f $(OPENOCD_PATH)$(JTAG).cfg -f $(OPENOCD_PATH)$(HOST_OPENOCD).cfg -f apps/waf/sflash_write/sflash_write.tcl -c "sflash_write_file $(APP1) $(APP1_SECTOR_ADDRESS) $(SFLASH_APP_PLATFROM_BUS) 0 $(SFLASH_APP_BCM4390)" -c shutdown #$(DOWNLOAD_LOG) 2>&1
endif
ifneq ($(APP2),)
APP0_DOWNLOAD: $(APP2_DOWNLOAD_DEPEDENCY)
$(QUIET)$(ECHO) Downloading APP2 ($(APP2)) at sector $(APP2_SECTOR_START)...
$(call CONV_SLASHES,$(OPENOCD_FULL_NAME)) -f $(OPENOCD_PATH)$(JTAG).cfg -f $(OPENOCD_PATH)$(HOST_OPENOCD).cfg -f apps/waf/sflash_write/sflash_write.tcl -c "sflash_write_file $(APP2) $(APP2_SECTOR_ADDRESS) $(SFLASH_APP_PLATFROM_BUS) 0 $(SFLASH_APP_BCM4390)" -c shutdown #$(DOWNLOAD_LOG) 2>&1
endif
Hi,
I need to send notifications from WICED device working in ble peripheral mode. However, I can't find any API to enable Client Characteristics Configuration Descriptor(CCCD).
There is API to send notification wiced_bt_gatt_send_notification(....); but that is not good method to send notifications.
Can anyone guide me how to enable CCCD ?mwf_mmfae
Show LessHello,
I am using SDK 3.3.1 and calling wiced_https_get to connect to a web server using SSL. Sometimes it fails to connect when there is not enough memory available on the heap. However, it returns the wrong error code 5035 (WICED_TLS_UNTRUSTED_CERTIFICATE).
wiced_https_get calls wiced_tcp_connect, which calls wiced_tcp_start_tls, which calls calls ssl_handshake_client_async in the BESL library. ssl_handshake_client_async is returning the 5035 code.
In this case there is not really a problem with the certificate; if I make more heap memory available it works. It probably should be returning 5003 (WICED_TLS_ERROR_OUT_OF_MEMORY). If the certificate really is incorrect then the function does correctly return the 5035 code.
-Paolo
Show LessI'v been using wiced_wifi_set_tx_power() in SDK 2.4.1
But I have to immigrate from SDK 2.4.1 to SDK 3.1.2.
There isn't wiced_wifi_set_tx_power() in SDK 3.1.2
I have to change wifi tx pwr level dynamically in SDK 3.1.2
Let me know how to change wifi_tx_pwr_level dynamically in SDK 3.1.2
Show LessI can't seem to find this anywhere