Wi-Fi Combo Forum Discussions
text.format{('custom.tabs.no.results')}
All,
As you may know the current SDK has a temp control demo. It allows you to talk to the xively cloud and send temp sensor information to the site from the eval board and vice versa.
As of May 1st xively is no longer creating new accounts (old accounts are "grandfathered" in), they claim to have a wait-list, but no estimate as to how long it would take.
We do have several Cloud Services supporting the Broadcom solution, so please reach out if you would like an introduction.
Apologize for the inconvenience. We will look into alternate solutions for our upcoming SDKs.
Show LessHi,
wiced_network_up returns SET_BLOCK_ACK_WINDOW_FAIL in the both the modes STA as well as SoftAP. I'm not able to figure out why it is happening.
As per my debugging, its setting something in the network controller and its not able to do that.
Is it a known issue and are there any fixes to this?
Show LessToday Avnet introduced the Avnet BCM4343W IoT Starter Kit powered by the Broadcom® WICED™ SDK with included cloud connectivity support to Amazon Web Services (AWS) IoT. The kit enables designers to quickly prototype and develop cloud-connected devices and then rapidly move to production with a pre-certified wireless SoC module.
Avnet has also created a short video to give engineers a preview of the board’s capabilities:
The Avnet BCM4343W IoT Starter Kit is priced at $49.95
Landing Page: Avnet CloudConnectKits
Purchase: Avnet AWS (AES-EVB-BCM4343W-G): Avnet Design Services - Custom AES-EVB-BCM4343W-G, - Avnet Express
Show LessHi Guys, Where to download WICED SDK 3.3.0 ?
Thanks !
Hi,
My purpose is downloading my new SDK 3.1.2 codes (sflash.bin, waf_bootloader-NoOS-NoNS-BCM9WCDUSI09-SDIO.elf, Arwen_v4_01_03-BCM9WCDUSI09, DCT.elf) to the board which has my old SDK 2.4.1 codes.
I have 2 ways to do that.
1) using WICED IDE: after using Arwen_v4_01_03-BCM9WCDUSI09 JTAG=jlink download download_apps run, I see below messages. Unfortunately I cannot succeed downloading.
Downloading Bootloader ...
Building apps lookup table
Download complete
Downloading DCT ...
"**** OpenOCD failed - ensure you have installed the driver from the drivers directory, and that the debugger is not running **** In Linux this may be due to USB access permissions. In a virtual machine it may be due to USB passthrough settings. Check in the task list that another OpenOCD process is not running. Check that you have the correct target and JTAG device plugged in. ****"
Downloading Application ...
"**** OpenOCD failed - ensure you have installed the driver from the drivers directory, and that the debugger is not running **** In Linux this may be due to USB access permissions. In a virtual machine it may be due to USB passthrough settings. Check in the task list that another OpenOCD process is not running. Check that you have the correct target and JTAG device plugged in. ****"
Downloading APP0 (build/Arwen_v4_01_03-BCM9WCDUSI09/binary/Arwen_v4_01_03-BCM9WCDUSI09.stripped.elf) at sector 1...
Downloading apps lookup table at 0x0000...
Resetting target
Target running
Build complete
17:19:57 Build Finished (took 1m:7s.797ms)
2) Batch file method (please see attached file we are using openOCD) : Our batch file is working good for SDK 2.4.1 codes. Unfortunately, when I want to use this way to upgrade board to the SDK3.1.2 codes, at first trial I see download failed message. After that I try again and even if I see download complete message, application code does not work. At the end my 3rd trial I succeed and and new SDK 3.1.2 application code works properly.
After downloading process succeeded, I try again WICED IDE, It works properly.
Waiting for your comments...
Best regards
Show LessHello Sir,
How about Max throughput of bcm943362 ?
have any project can do throughput test ?
I use sdk3.3.1 , modify the snip.udp_transmit and snip.udp_receive project
but I test throughput only 11k bytes.
I used wiced_rtos_register_timed_event(....) , setting UDP_MAX_DATA_LENGTH = 1024, UDP_TX_INTERVAL = 80ms
Can give me suggest ?
Thanks you Sir !!
Show LessHi,
I am getting the following error whenver i am trying to use interface stlink.... Please help
Licensed under GNU GPL v2
Downloading Bootloader ...
For bug reports, read
http://openocd.sourceforge.net/doc/doxygen/bugs.html
Error: The specified debug interface was not found (stlink)
The following debug interfaces are available:
1: parport
2: dummy
3: ft2232
4: ft2232_swd
5: usb_blaster
6: amt_jtagaccel
7: gw16012
8: presto
9: usbprog
10: jlink
11: vsllink
12: rlink
13: arm-jtag-ew
Runtime Error: .//tools/OpenOCD/stlink.cfg:30:
in procedure 'script'
at file "embedded:startup.tcl", line 58
in procedure 'interface' called at file ".//tools/OpenOCD/stlink.cfg", line 30
tools/makefiles/standard_platform_targets.mk:44: recipe for target 'download_bootloader' failed
make.exe[1]: *** [download_bootloader] Error 1
make.exe[1]: *** Waiting for unfinished jobs....
Makefile:185: recipe for target 'main_app' failed
make: *** [main_app] Error 2
Show LessDear All:
My WICED device is always crash and reboot when web server is booted.
I check all system and no way to fix.
Can you give me a hint which cause a crash?
How can know crash is generated by hard fault, time out ....?
Is there any exception to printf a error message when crash?
hard fault, time out or any kind of reason why system is crash?
Show LessI understand the WICED SDK provides OTA for firmware upgrades. However, the STM 32 bootloader supports the DFU protocol (Device Firmware Upgrade) but it is not clear how to use it with the WICED.
I am wondering if I can get some directions and advise on how to use DFU in a WICED design. It seems very important not only in development, as DFU is a widely used protocol with host software available for a variety of OS.
Thanks.
Show LessI've downloaded the lated WICED SDK 3.3.1 . There is a usefull api.html file to search the documentation. Unfortunatly there is no .pdf files in the installed SDK\doc directory . How to get All the Documentation which should be in the doc directory ?
Thanks , Michel V.
Show Less