Wi-Fi Combo Forum Discussions
text.format{('custom.tabs.no.results')}
Hello,
I would like to pair the WiFi module with many APs. Is it possible to add a new AP to the AP_LIST ? Can you please provide also an example for this procedure ?
Thank you!
Show LessI need something similar to wiced_time_get_iso8601_time, but to be able to set time zone.
thank you
Show LessHello
I have a developer board with a dht11 (umidity & temperature sensor)
How can I get the information ,maybe samplee code
like this one ?
wiced_gpio_input_get( WICED_GPIO_XX)
Show LessI am pretty new to WICED, and writing a lot of new code. However, I am finding the environment a very difficult one in terms of common practices like unit testing. I noted that throughout the make files, there are references to unit tests. For example library/daemons/DHCP_server has a makefile that contains definitions such as $(NAME)_UNIT_TEST_SOURCES along with a list of unit tests.
However, I cannot for the life of me find any method to run these tests, nor any information on how to write my own unit tests for new code I am developing.
This is a huge problem for us. Can you provide any insight into what kind of unit test capabilities are built into the WICED SDK and how to trigger them? Or, point me to any documentation I may have missed?
Show LessThe 3.3.1 SDK readme mentions the following restrictions:
* Platform Restrictions:
BCM943341WCD1
- Wi-Fi Direct not support
- SPI bus not supported
Are there plans to add support for Wi-Fi Direct and SPI in a future release?
Show LessHello,
when I try to run a demo on the board, I cannot connect to my wlan hot spot ( iphone).
target : demo.aws_iot.shadow-BCM94343W_AVN download run
Starting WICED v3.4.0-AWS
Platform BCM94343W_AVN initialised
Started ThreadX v5.6
Initialising NetX_Duo v5.7_sp2
Creating Packet pools
WWD SDIO interface initialised
WLAN MAC Address : B0:38:29:3D:3C:3D
WLAN Firmware : wl0: Nov 25 2015 12:57:14 version 7.45.45.1 (r602358) FWID 01-1920c040
Please wait, connecting to network...
(To return to SSID console screen, hold USER switch for 5 seconds during RESET to clear DCT configuration)
*******************************************************
Config SSID : WICED_AWS
Password : 12345678
IP Address : 192.168.0.1
*******************************************************
my config wifi_config:
#define CONFIG_AP_SSID "WICED_AWS"
#define CONFIG_AP_CHANNEL 1
#define CONFIG_AP_SECURITY WICED_SECURITY_WPA2_AES_PSK
#define CONFIG_AP_PASSPHRASE "12345678"
/* This is the soft AP available for normal operation (if used)*/
#define SOFT_AP_SSID "WICED Device"
#define SOFT_AP_CHANNEL 1
#define SOFT_AP_SECURITY WICED_SECURITY_WPA2_AES_PSK
#define SOFT_AP_PASSPHRASE "WICED_PASSPHRASE"
/* This is the default AP the device will connect to (as a client)*/
/* This is the default AP the device will connect to (as a client)*/
#define CLIENT_AP_SSID "my iPhone"
#define CLIENT_AP_PASSPHRASE "xxxxx"
#define CLIENT_AP_BSS_TYPE WICED_BSS_TYPE_INFRASTRUCTURE
#define CLIENT_AP_SECURITY WICED_SECURITY_WPA2_MIXED_PSK
#define CLIENT_AP_CHANNEL 1
#define CLIENT_AP_BAND WICED_802_11_BAND_2_4GHZ
/* This is the network interface the device will work with */
#define WICED_NETWORK_INTERFACE WICED_STA_INTERFACE
But when I run a sample without
aws_config.c & aws_common.c
like in target : demo.aws_iot.pub_sub.publisher-BCM94343W_AVN download run
I have access to my hotspot
what i my problem ?
Show LessHello All,
I have three questions about MQTT protocol and its usage in WICED.
1.As I understood, there's no timeout mechanism in MQTT protocol.
However in Wiced API MQTT snips, WICED_MQTT_TIMEOUT is defined and in AWS demos MQTT_REQUEST_TIMEOUT is defined.
Is this timeout something you added such that after some time it'll return error? Or Is it a part of the MQTT protocol which I missed?
2.The ACK mechanism of MQTT is different for different QoS choices. Doesn't MQTT run over TCP, do we really have to run an ACK mechanism? What improvement does this mechanism add on top of TCP?
3.As I understood with AWS, we can only use QoS 0 or 1 (the AWS demo also uses QoS 1), what would you propose to get QoS 2 functionality while using AWS?
4.Is there a sample application which implements MQTT over TLS?
Thanks.
Show LessHow do I get the mfg-test.bin firmware into external flash?
I know I can run the sflash_write program by doing the following:
SFLASH=dct-download.
I need to get the WiFi firmware into external flash because I cannot fit it in the ST micro.
Thanks,
Ben
Show LessHi,
I set up a ap router which has dhcpv6 server and build "test.console-BCM943362WCD4-ThreadX-NetX_Duo-SDIO download run" to my EVB(BCM943362WCD4).
I can only get IPv4 address from status and also check ap's dhcpv6 table.
There is no global IPv6 address in EVB.
Best regards,
Kenny
Show Less