Wi-Fi Combo Forum Discussions
Hey,
We are currently investigating the option of using WICED Wi-Fi / BLE components in a future design.
It leaded us for a couple of questions:
- Can someone please recommend of a component that is intended for new Wi-Fi + BLE designs?
- Can we purchase a BCM WICED component or is it available in partner modules only?
- Which components include an internal MCU for custom application and which require an external HOST MCU?
We would appreciate your help,
Thanks,
Nir
Show LessHey,
We are looking for a hands-on workshop / seminar for Broadcom WICED Wi-Fi / BLE products / modules.
Is there any event about to take place in the coming months? where can we find a list of the planned events?
Thanks!
Nir
Show LessHi All,
If our app is in internal flash (ex. STM32F4xx ) instead of external flash does OTA still works ?
I have this question because OTA use wiced_framework_app_write_chunk() but under the API it seems only apply to sflash calls (external flash). So I don't know how it works to internal flash write.
If I'm wrong on this please correct me.
Show LessAs a central BLE, I want to discover the services of the device I am connected to.
It works most of the time except that sometimes I get a GATT_DISCOVERY_CPLT_EVT event type with the status 0x85 (WICED_BT_GATT_ERROR).
Show LessI am able to do the wifi testing on command prompt using wl tool (wl4343WA1.exe).
we have the source code of wl tool. which is located at 'libraries/test/wl_tool'
I want to do the wifi testing on command console (test.console app) ?
Is it possible to do it ?
Would anyone help me, how to do it ?
Show LessI want to run the bat from wiced sdk
.
How can i do this ?
can anyone help us?
hello,
Does WICED really support SPI slave APIs as i don't see any implementation for spi_slave_init function at all.
Can anyone please share SPI slave implementation code for any of the WICED platform.. I have written the code myself, for some reason i am not able to see the recieve interrupts or also polling also doesnt reveal any data..
Thanks,
Raghu
Show LessScanning code that uses the wiced_wifi_scan_networks api works fine if run before creating an AP association.
But if an AP is brought up, the wiced_wifi_scan_networks function returns WICED_SUCCESS when called, but the scan
does not find any AP's even though there are many AP's present.
The call to wiced_wifi_scan_networks is from a main thread and not from a callback.
Show LessWe are using Murata Type1DX having BCM4343w. When we program the module to work in AP mode over WPA2 we see that we are able to connect devices like iPhone and windows machines. But we are not able to connect android based phones. The android phone reports that the association did not succeed
We see that when the AP is configured in WEP mode we are able to connect successfully connect android devices.
Is this a known issue with BCM4343?
Show LessHello,
We have code that only works when -debug is specified in the build string. After some reading, I found that -debug disables optimization. Is there a way I can disable optimization in the build string explicitly? I would like to verify this is the cause of strange behavior in code (delayed UART responses after performing a DMA ADC reading).
Thanks,
Ben
Show Less