Wi-Fi Combo Forum Discussions
We need to create a 802.1X connection from WICED thru an AP using a RADIUS server for authentication.
We have reviewed some of the source code in the WICED\WICED-Studio-4.0\43xxx_Wi-Fi\WICED\security\BESL section and can see many supporting functions. Is there any documentation on this available.
We are using WICED 4.0.7.58 on the 43340 platform from Inventek Systems.
Thanks in advance.
Greg
Show LessI use BCM43438( with WICED SDK 3.7.0 ) as a BLE central device to scan ble broadcasting data and print with Serial.It will show the data broadcasting by the ble deivce surrounded.
In other hand ,I have some nRF BLE mesh device.When I use LightBlue to connect one mesh device and write some data to it,it will broadcast some message.I use a sniffer to scan and can find that message but the BCM43438 can not get that message(It didn't printed by the Serial)
It's so strange and can somebody help?mwf_mmfaeakyboontjakewtorres
Show LessHello,
What Cypress board do you recommend for a beginner to start programming IoT applications?
Which are the IoT platforms agreed by Cypress IoT kits?
Can we connect the kit to IBM Watson IoT or PTC/ThingWorx?
Thank you
Corneliu
Show LessI have been reading the discussions on the forum about OTA and OTA2 updates.
If I am not wrong, OTA2 is currently not available for BCM94343W
OTA example in snip folder makes use of a web server where the user picks the new firmware image.
Are there also examples for automatic updates (WITH OTA) where the app connects to a server and downloads the image automatically?
OTA2 example works like that but it's unfortunately not available for BCM94343W.
thanks
rifo
Show LessHi everyone
I'm new at this forum.
I would like to know which is the minimum software background one need to get started coding app with the SDK.
I am currently writing code in C for PSoC 3 and PSoC 5LP
Thank you very much.
Show LessHi
I'm using WICED Wifi SDK 3.5.2 and I'm trying to create HTTP/2 client on EMW3162.
Did WICED Wifi support HTTP/2 protocol? If yes, where can I find example how to use it. If no, when can I expect that HTTP/2 will be supported?
/Grzegorz
Show LessHi
Web Demo
- BCM4390WCD Serial-2-WIFI module
- SDK 3.7.0
- Live Demo
1) Serial-2-WIFI Module Demo : http://damosys.com:8001
2) Light Controller Demo : http://damosys.com:8002/main?5
3) Temperature & Humidity Demo : http://damosys.com:8003/main?5
Cloud Server for Data : DAMOSYS Inc., - ThingSpeak
login account
ID : admin
PWD : admin
TKS
Show LessHi,
I'm studying the appropriate Wi-Fi country code for several countries.
For example, west Europe countries (UK, France, Germany, Italy, Portugal and Spain) can be covered by UK country code.
Do you have any table or list above?
Or can you provide the channel table of 4390x for each country code?
e.g. JP: 1-13, 36-48, 52-64, 100-140(DFS)
US: 1-11, 36-48. 52-64(DFS), 100-140(DFS), 149-465
regards
Show Lessin my application, i am using MQTT protocol and and it works fine for half and hour than it does not work properly.
However i have kept keep alive time for an hour and i am sending ping massage on PINGREQ topic at regular interval
so can i get any solution for the same?
Show LessHello,
I have been trying to get WICED Studio 4.0 running on my MacBook with Mac OS Sierra.
I keep getting this error when I try to compile the scan snip.
Building Bootloader
WICED/platform/GCC/math_newlib.c: In function 'sin':
WICED/platform/GCC/math_newlib.c:53:5: internal compiler error: Illegal instruction: 4
x -= ( (int) ( x / ( 2 * PI ) ) ) * 2 * PI;
^
libbacktrace could not find executable to open
Please submit a full bug report,
with preprocessed source if appropriate.
See <http://gcc.gnu.org/bugs.html> for instructions.
make[3]: *** [build/waf.bootloader-NoOS-KIG100_HW3/Modules/WICED/platform/GCC/math_newlib.o] Error 1
make[3]: *** Waiting for unfinished jobs....
make[2]: *** [main_app] Error 2
make[1]: *** [bootloader] Error 2
make: *** [main_app] Error 2
The error has been discussed in other threads, but I have not been able to get any clear indication on how to fix this.
ubuntu 16.04 x64 - WICED SDK 3.7.0.3 math_newlib.c error workaround
Illegal Instruction: 4 error on Mac OS X El Capitan with Wiced Wifi SDK 3.5.2
Anybody which have experienced this error on Mac and has been able to fix it?
Regards
René Josefsen
Show Less