Wi-Fi Combo Forum Discussions
I'm trying to run the snip.bluetooth.bt_dualmode_server project.
I have tried downloading on the the BCM94343W_AVN board and the Future Electronics NEB1DX_01 board (modifying the mk file for the avn project) shown here: NEB1DX-01 | Nebula 1.0 IoT Cloud Ready Development Board for IoT Applications | FUTURE ELECTRONICS DEV TOOLS - Future …
The project builds and downloads ok, but if i try to connect using the SPP Pro app on Android (using a stock Nexus 6 running Android 7.1.1) i can pair to the device but not connect to it.
I have attached the terminal logs from both projects in case they could be of any use. Is there something i need to do to get the project working?
This was tested on WICED 6.0.1.5
Thanks
Graham
Show LessHi,
Can I get the CYW43907 gSPI Slave Peripherals operation related data?
Like the gSPI Registers, signal timing, command structure...
Thanks.
Randy
Show LessI'm trying to use avs, but it looks like SDK 5.0.1 has /libraries/audio/avs_client and disappeared in SDK 6.0.1.
Could you tell me why it was deleted?
Show LessI have two CYW943907AEVAL1F Demo, I download respectively udp_receive project and udp_transmit project to one demo board. The receiving board is power-on firstly, then the transmitting board is power-on. But the receiving board display " Waiting for UDP packets... ", the transmitting board display " sent: 10". The receiving board does not receive the UDP packet from the transmitting board. Why? How to fix it?
Show LessI am looking for company/Embedded Firmware engineers , who is familiar with WICED Wi-Fi and BLE to develop a firmware which can connect to Mobile and cloud
Show LessHi,
We found enable wifi has impact on the received BLE RSSI values.
The test is pretty simple:
Make the wiced device scan the nearby tags. (Put a tag in fixed position as reference for the test)
When wifi is disabled, the observed ble tag RSSI looks fine. (use wiced_bt_ble_observe() or wiced_bt_ble_scan())
When wifi is enabled (either join a AP or wiced device being a AP), the observed ble tag RSSI deviation becomes too large.
This issue makes the device not able to be used for detecting object location.
Tested on USI-BM22 (43438) and SPIL-N08 (4343W) with latest SDK.
Show LessHello,
I have been checking the available modules and it seems that for a reliable OTA / OTA2 process, the only alternative is CYW43907 based modules.
I have checked the module purchase guide but wasn't able to find a CYW43907 module that I can order online.
There is CYW943907AEVAL1F but it's the development kit.
Do you guys have any info regarding this?
thanks
rifo
Show LessThe schematic provided on the website and even in WICED SDK are same .The schematic doesn't include many pin, headers, ICs etc .
If anyone can provide me the complete schematic for this evaluation board.
The mentioned schematic is attached below.
Show LessHi,
I want to use two BCM943907WCD2 devices and one is server(or gateway) ,the other is client.
The AP fails to start DHCP service at wiced_start_dhcp_server() because I define the interface as WICED_ETHERNET_INTERFACE .
How can I get the right configuration to run a BCM943907WCD2 platform as an ethernet server with DHCP function?
Could anyone help?
Show LessHi.
I installed wiced studio 6.0.
When you run the IDE, nothing appears on the left side of the Project Explorer.
When I installed the wiced-sdk 3.0 IDE, I found sample, platform .. in the Project Explorer section.
In wiced studio 6.0, the development board should be connected to the PC, but is it usable?
I want to know why nothing appears in the Project Explorer section.
It seems that the SDK file is not properly installed.
There is only tools folder in "d: \ WICED-Studio-6.0 \ SDK \ 43xxx_Wi-Fi" folder.
Is this correct?
The folder "d: \ WICED-Studio-6.0 \ SDK" contains only 43xxx_Wi-Fi, common, Doc, Drivers, RemoteSystemTempFiles, test, and wiced_tools folders.
I have posted this question before, but I do not have an exact answer, so please contact me again.
Please help me.
Show Less