Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Wi-Fi Combo Forum Discussions

Anonymous
Wi-Fi Combo
When writing to a random place in sflash on most sflash chips the process is very slow on some chips the data written will be corrupted. This can be e... Show More
MaCa_2922036
Wi-Fi Combo
Hello,I met an issue with the lib http and http_client with the function which get the Http answer received after sending a HTTP GET request: The func... Show More
harelTur
Wi-Fi Combo
Hi  I try to init I2c and I dont see any signal of clock of I2c  My code :  static const wiced_i2c_device_t BARO_I2C ={.port = BARO_I2C_PORT,.address ... Show More
lefeno
Wi-Fi Combo
According to my understanding, the SECURE BOOT option is written to the OTP address field, and maybe is used in the ROM bootloader only to decrypt and... Show More
MilesHsu
Wi-Fi Combo
I want to download the Wiced 4.0.1 to develop my product , I find the link: https://community.cypress.com/t5/WICED-Studio-Wi-Fi-Combo/WICED-Studio-4-0-1-has-been-released/m-p/69201... Show More
Félix_T
Wi-Fi Combo
I am trying bring up a new board that we have made using an Azurewave AH-306. When scanning, the chip immediately returns from the scan with the respo... Show More
Anonymous
Wi-Fi Combo
We are using a murata SN8000 module connected via SDIO operating with 48 Mhz to a Cortex-M3 LPC1837. We are using a WWD ported from the SDK 3.1.2 (inc... Show More
mzimmers
Wi-Fi Combo

Hi all -

Does anyone know how I could get a copy of version 2.4.1 of the WICED SDK?

Thanks...

Calvin
Wi-Fi Combo
Hi there, I just installed the latest version WICED Studio for macOS 11.4. My Java version is: java version "1.8.0_301" Java(TM) SE Runtime Environmen... Show More
GT
Wi-Fi Combo
Hello, I want to do WiFi radio tests on my board, where there is only a STM32F7xx connected with STDIO to a CYW43455. I can not access to the STDIO to... Show More
Forum Information

Wi-Fi Combo

Discussion forum regarding WICED Studio Wi-Fi Combo topics.