Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Wi-Fi Combo Forum Discussions

ToLa_2193696
Wi-Fi Combo
Per the previous thread here: WICED Studio 6.2 does not install correctly I have a similar problem on OS X. It seems that the 43xxx_Wi-Fi folder is no... Show More
save_3366371
Wi-Fi Combo
Hello, I have cc3200audboost and I have cyw943907aeval1f evaluation kit. I need to stream audio/voice over wi-fi using these two boards using an I2S i... Show More
MiRo_263836
Wi-Fi Combo
What is the power consumption of the R4 Core @ 320Mhz when not using the radio?I will be doing a lot of work with the R4 in active mode and only trans... Show More
NaTa_2243041
Wi-Fi Combo
Hello,I have CY8CKIT-062-WiFi-BT.I would like to control the power mode of PSoC 6 using WICED Studio 6.2.Do you have samples that will be helpful?PSoC... Show More
NiMc_1688136
Wi-Fi Combo
Is it possible to set the application Major/Minor version numbers from a file, such as a header, versus defining it in the build target?I want to go f... Show More
user_108962310
Wi-Fi Combo
I am having an issue with an old version of the SDK, 3.1.2, with devices that are presently in the field. I am having an unexplained issue wherein I g... Show More
user_108962310
Wi-Fi Combo
I am having an issue with WWD initialization by using wiced_core_init() separately from wiced_wlan_connectivity_init() .I am getting a return of TIMEO... Show More
AxLi_1746341
Wi-Fi Combo
mifo​I just found you changed the 6.2 release to 6.2.1https://community.cypress.com/thread/34443What is the difference between 6.2 and 6.2.1?I don't s... Show More
Anonymous
Wi-Fi Combo
Firmware version: wl ver1.8 RC0.0wl0: Apr 10 2018 00:42:50 version 13.10.271.99 (r687870) FWID 01-2151702eI am attempting to set up the new keep-alive... Show More
Anonymous
Wi-Fi Combo
Having a problem at 'Choose IDE Folder Location' step:There's about 1TB of space on this drive, so it would be nice to know what's really wrong here. ... Show More
Forum Information

Wi-Fi Combo

Discussion forum regarding WICED Studio Wi-Fi Combo topics.