Wi-Fi Combo Forum Discussions
I want to do some porting to other MCUs, What should I do?
Hi ,
Do you have a guide provide to user about how to add a new platform in WICED?
I would like to porting a new platform to WICED, but I don't know how start.
Thanks!
Show LessHi
I have asked the below question
I am sending the pkteng_start 00:11:22:33:44:55 tx 100 1024 0 to test the WLAN kit in 802.11ac standard(5GHz band and 40MHzBW).While sending the packet,1024 bytes of data is going along with all payload data,header and preamble.How to find out payload data alone in the whole 1024 bytes of data?Could u please help me hoe to finding out it.
You have replied like below one:
You can use a sniffer like wireshark for that purpose to check the payload.
I am not able to understand your suggestion.Could you please explain me again
Thanks&Regards,
harshini
Show LessHi,
This is discussion is regarding part no: CYW54907KWBGT (WICED™ IEEE 802.11 a/b/g/n/ac SoC with an Embedded Applications Processor).
As per the datasheet (http://webinr.keysight.com//Docs/202/88/02/CYW54907_WICED_IEEE_802.11_a_b_g_n_ac_SoC_with_an_Embedded_Applications_Proce… ), the package for this part is 4.583 mm x 5.533 mm, 316-pin WLCSP. But there is no information regarding ball/pin placement in the datasheet.
Please provide us detailed physical drawing for this part.
Also, I was checking CYW954907AEVAL1F Evaluation Kit (http://www.cypress.com/documentation/development-kitsboards/cyw954907aeval1f-evaluation-kit ) for this part. As per the gerber and schematic of this part. The package size is 10 mm X 10 mm with 136 pins).
Please confirm the part size and number for this part?
Thanks & Regards,
Sunny Watts
Show LessHello All,
I am getting an error in IP configuration using One AP from Belkin. But while sendinDHCP discover packet I am able to see some block ACK request and responses. And I am thinking that due to the AP is not able to send offer packet and so IP is failing. Is there any configuration in the SDK that I can disable this Block ACK from the cypress module. I am attaching the wireless capture and UART logs for reference. I am using SDK version 6.2.1.
Thanks
Milan
Show LessI'm testing with WICED SDK 6.2.1 and the demo app "restful_smart_server".
It is possible to make a ble scan and get the results, but when trying to connect to a peripheral it does not work!
The connection fails every time.
When using the demo app "restful_smart_server" of WICED SDK 5.2.1 everything is working (scan, connect, read, write, ...)!
It seems, that WICED SDK 6.2.1 has some major problems with BLE (see also WiFi and BLE are not working together (tags: link up, link down, BLE) ),
and can't be referred to as "production ready".
best regards,
Gregor Bader
I have a issue in the function wiced_network_up(). It take long time( abt 4s -> 14 seconds) to connect successfully.
And I see that it take so much time because it must wait for the IP to be ready.
The flow as below
So we would like to know is there any way to improve waiting time of IP ready ?
Show LessHow to use the AP example or anyother example and pass internet traffic via a cell module (UART/USB)
Hi grsr
After apply the patch from below link
https://community.cypress.com/thread/35745
I have chance to get EAP-TLS work.
But I found the join_ent fails after leave_ent.
It seems not reliable...
Can you check the issue?
With FreeRTOS build:
> join_ent LAB-WPA2-ENT eap_tls bob hello eap mschapv2 wpa2
Joining : LAB-WPA2-ENT
Successfully joined : LAB-WPA2-ENT
Obtaining IPv4 address via DHCP
IPv4 Network ready IP: 192.168.1.111
Successfully retrieved the session information 0
> leave_ent
leave test: ok
> join_ent LAB-WPA2-ENT eap_tls bob hello eap mschapv2 wpa2
Joining : LAB-WPA2-ENT
Failed to join : LAB-WPA2-ENT
Joining : LAB-WPA2-ENT
Failed to join : LAB-WPA2-ENT
Joining : LAB-WPA2-ENT
Failed to join : LAB-WPA2-ENT
Join result 1055:
failed
! mbedtls_ssl_handshake returned -0x2
Error setting supplicant event handler 2
>
With ThreadX/NetX_Duo build:
> join_ent LAB-WPA2-ENT eap_tls bob hello eap mschapv2 wpa2
Joining : LAB-WPA2-ENT
Successfully joined : LAB-WPA2-ENT
Obtaining IPv4 address via DHCP
DHCP CLIENT hostname WICED IP
IPv4 network ready IP: 192.168.1.111
Setting IPv6 link-local address
IPv6 network ready IP: FE80:0000:0000:0000:462C:05FF:FE80:65FC
Successfully retrieved the session information 0
> leave_ent
leave test: ok
> join_ent LAB-WPA2-ENT eap_tls bob hello eap mschapv2 wpa2
Joining : LAB-WPA2-ENT
Successfully joined : LAB-WPA2-ENT
Obtaining IPv4 address via DHCP
DHCP CLIENT hostname WICED IP
IPv4 network ready IP: 192.168.1.111
Setting IPv6 link-local address
IPv6 network ready IP: FE80:0000:0000:0000:462C:05FF:FE80:65FC
Successfully retrieved the session information 0
> leave_ent
leave test: ok
> join_ent LAB-WPA2-ENT eap_tls bob hello eap mschapv2 wpa2
Joining : LAB-WPA2-ENT
Failed to join : LAB-WPA2-ENT
Joining : LAB-WPA2-ENT
Failed to join : LAB-WPA2-ENT
Joining : LAB-WPA2-ENT
Failed to join : LAB-WPA2-ENT
Join result 1007:
failed
! mbedtls_ssl_handshake returned -0x2
>
Show Less