Announcements

Help us improve the Power & Sensing Selection Guide. Share feedback

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Wi-Fi Combo Forum Discussions

user_875031
Wi-Fi Combo
1. I wan to just build one bin ,not contain the  bootloader.bin,what should I do?2. if I just build one app bin ,what should I  build the DCT in the a... Show More
HIUR_3769846
Wi-Fi Combo
I have same issue in my application. In my situation, I build with "ota2_manuf_download" option, and after that I can build with ota2_download. Howeve... Show More
cohuc_3807591
Wi-Fi Combo
I have an application that will receive infrequent commands over at TCP connection. I was wondering if there was a way to have a thread that handles t... Show More
MiKi_4159711
Wi-Fi Combo
iperf3 tests are run with UDP between 2 Pi 3B boards over the on-board WiFi ( channel 6 = 2.437 GHz)Server Pi is set up as Access Point (hostapd/dnsma... Show More
Us16_3774766
Wi-Fi Combo
I am testing snip.httpbin_org on CWY943907AEVAL1F. I use WICED-Studio-6.2.The original sample work correctly. I modified the  original source code to ... Show More
BeDe_2507241
Wi-Fi Combo
I am using the following function to join an AP:wwd_result_t wwd_wifi_join_specific( const wiced_scan_result_t* ap,                                   ... Show More
supac_4156951
Wi-Fi Combo
Need information for Callback registration for events like  Link/connection up/down , wifi hardware error,etc. Can Event be registered in wiced  for w... Show More
BaGo_4138971
Wi-Fi Combo
Hi All,I'm new to the Wiced devices. We are using BCM943907 device in our product. I installed the WICED-Studio-6.2.1.2-IDE-Installer to my window 10 ... Show More
user_875031
Wi-Fi Combo
I wan to use IAR toolchain to build then wifi project , so my Make target is "snip.scan-BCM943362WCD6 IAR=1".However it take some Erro like the flowin... Show More
NiMc_1688136
Wi-Fi Combo
SDK 6.2.0CYW43907FreeRTOS + lwIPI have been using wiced_tcp_send_packet without any issues until i tried to send larger packets. I then switched to wi... Show More
Forum Information

Wi-Fi Combo

Discussion forum regarding WICED Studio Wi-Fi Combo topics.