Announcements

Help us improve the Power & Sensing Selection Guide. Share feedback

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Wi-Fi Combo Forum Discussions

BaGo_4138971
Wi-Fi Combo
Hi All,I'm using SDK6.1. I'm using "make snip.pers-BCM943909WCD1_3.B1-ThreadX-NetX_Duo-debug ota2_download" to build and load the source code.I want t... Show More
bohic_4007501
Wi-Fi Combo
Hi,We'd like to use CYW43455 module in one of our product design in a FCC Class B environment. Is there any reference design guide available from Cypr... Show More
NiMc_1688136
Wi-Fi Combo
I am trying to run the snip\ping_deepsleep example with FreeRTOS and LWIP. The application is crashing (hitting assert) right after getting the DHCP a... Show More
renoc_4290386
Wi-Fi Combo
Hi,   During my tests SMTP, we used several email servers. In one of them we noticed that the TLS protocol simply hangs.   This happens while using sm... Show More
Anonymous
Wi-Fi Combo
Hi all,I have a requirement to read the Wifi password on a WICED device, then pass it to another WICED device using a non-wifi communication link. How... Show More
user_4252696
Wi-Fi Combo
I am working on a project using an the ISMART43340-C from Inventek Systems. This evaluation board has a CYW43340 module. This module is suppose to rep... Show More
ViSh_4113431
Wi-Fi Combo

which two of the default I/O controls of CYW54907 are specifically used to control T/R switch?

ViSh_4113431
Wi-Fi Combo

what's 1ps module I/Os to control the Pin 233 and pin 239 TR switch?

jina_4171326
Wi-Fi Combo
hi,currently i'm using CYW954907AEVAL1F development board with wiced IDE. it's based on CYW54907 chip which is inside LBWA1UZ1PS-241 module.but now i ... Show More
KeBe_3995361
Wi-Fi Combo
Hello support,I have a doubt related to Vbat and Vddio:    - What is the purpose of Vbat? And the purpose of Vddio?   - What is the difference between... Show More
Forum Information

Wi-Fi Combo

Discussion forum regarding WICED Studio Wi-Fi Combo topics.