Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
jalic_4332871
Level 1
Level 1

I am using two bcm 43438A, the two devices are putted into a shield box, then I  tested them in wifi mfg mode. One device sends 1000 package, the other one only receives around 960 packages.

Below is the  wl version

# wl ver                                                                                                                        

6.37 RC32.0                                                                                                                       

wl0: Apr 23 2015 20:40:36 version 7.46.3 (r551729 WLTEST) FWID 01-af384561                                                        

/ #

THE SENDER COMMANDS

1. ifconfig wlan0 up

2. wl down

3. wl mpc 0

4. wl country ALL

5. wl up

6. wl scansuppress 1

7. wl band b

8. wl channel 7

9. wl nrate -r 11

10. wl txpwr1 -o -d 30

11. wl pkteng_start <MAC> tx 100 1000 1000

12. wl phy_forcecal

THEN RECEIVER COMMANDS

1. ifconfig wlan0 up

2. wl down

3. wl mpc 0

4. wl country ALL

5. wl up

6. wl scansuppress 1

7. wl band b

8. wl channel 7

9. wl nrate -r 11

10. wl frameburst 1

11. wl phy_watchdog 0

12. wl pkteng_start <MAC> rx

13. wl reset_cnts.

wait 1000 packages are transmitted.

14. wl counters | grep pktengrxdmcast

The result: only around 960 packages received. What may cause this problem.

0 Likes
1 Reply
Zhengbao_Zhang
Moderator
Moderator
Moderator
250 sign-ins First comment on KBA 10 questions asked

hello:

What is the reason to use so big power setting?

wl txpwr1 -o -d 30

0 Likes