- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi
I have installed Wiced 6.1 (6.4 simply doesn't install the platform folders). And then installed Peripheral Driver Library 3.1 and also installed CY8CKIT062WiFiBT setup.
When I try to download and run the "scan" Wifi example on the CY8CKit-062 Wifi+BT, I get errors stating OpenOCD failed.
Please help, I just can't get things running.
Moreover WICED 6.4 doesn't even install correctly, it shows no platforms in the make target.
Thank you
Solved! Go to Solution.
- Labels:
-
ispn:39620:1:0
-
l1:314:1:0
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello MrMa_286121
WICED 6.4 does install without any issues and all the platform folders required to use the WiFi BT pioneer Kit are also installed. Did you follow the steps as mentioned in WICED-Studio 6.4.0 Installer (Windows). Was the config.eml in the same folder as the .exe file? You need to change the kitprog 3 to kitprog 2 using the fw-loader for the platform to work with WICED. For more information, please refer to : GitHub - cypresssemiconductorco/Firmware-loader: A command-line tool to update KitProg low-level pro...
Thanks
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello MrMa_286121
WICED 6.4 does install without any issues and all the platform folders required to use the WiFi BT pioneer Kit are also installed. Did you follow the steps as mentioned in WICED-Studio 6.4.0 Installer (Windows). Was the config.eml in the same folder as the .exe file? You need to change the kitprog 3 to kitprog 2 using the fw-loader for the platform to work with WICED. For more information, please refer to : GitHub - cypresssemiconductorco/Firmware-loader: A command-line tool to update KitProg low-level pro...
Thanks