Wi-Fi problem in WICED Studio 5.0.0.33?

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
GrTo_1576836
Level 2
Level 2
10 sign-ins 5 sign-ins 10 replies posted

I have two boards with two different Cypress chips, one is 4343W and other is 43438.

The standard snip.scan works under WICED Studio 4.1.1.8 on both boards; nearby APs are displayed in the scan list

The standard snip.scan doesn't work on either board under WICE Studio 5.0.0.33; initialization messages are printed but nothing appears in the scan list

Similar issue with test.console -- scan works on both boards under 4.1.1.8 but scan results are empty under 5.0.0.33 on both boards.

Are there any known problems with the Wi-Fi components in 5.0.0.33?

Thanks

0 Likes
2 Replies
JaeyoungY_71
Employee
Employee
First comment on KBA 25 solutions authored 10 solutions authored

Hello Greg,

I've just tried snip.scan with a BM94343WWCD1 eval board and scan is working fine for me. What are you using as your target name? Can you upload the terminal output you are getting?

Thanks,
Jaeyoung

pastedImage_0.png

AkFu_2032386
Level 1
Level 1
First like given Welcome!

greg_1576836

Could you enable the following error log options and check initialization messages?

include/wiced_defaults.h

#define WPRINT_ENABLE_NETWORK_ERROR

#define WPRINT_ENABLE_RTOS_ERROR

#define WPRINT_ENABLE_WICED_ERROR

#define WPRINT_ENABLE_WWD_ERROR

#define WPRINT_ENABLE_PLATFORM_ERROR

0 Likes