Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
yowuc_3086231
Level 1
Level 1

I want to use the CYW43907 working in temperature -30 to 70 centigrade,

So prepare to evaluate it with this Eval Kit.

What's the Work Temperature of CYW43907 Eval Kit?

Can it work in -30 to 70 centigrade?

0 Likes
1 Solution

The Eval Kit has not been tested for this temperature range but the chip/module has been tested as noted in the datasheet.

View solution in original post

0 Likes
4 Replies
RaktimR_11
Moderator
Moderator
Moderator
500 replies posted 250 replies posted 100 replies posted

If you check Table 17 of 43907 datasheet (https://www.cypress.com/file/298236/download ), you can find the range to be -30 to +85 centigrade. So, the range you mentioned should be okay.

Thanks for your kindly reply。

Maybe I don't describe it clearly.

I just want to know the work temperature of CYW43907's Eval Kit (CYW943907AEVAL1F), not the device chip.

0 Likes

@prog_3086231

As per the environmental ratings on the 54907 datasheet (Table number 16 on Revision C and Table number 17 on Revision J), -30 to +85 ℃ is the Ambient Temperature in which the device was operational/functional.

Which means, the CYW54907 Eval Kit can work between -30 to +85℃

As per your question "Can it work in -30 to 70 centigrade?"

the answer is YES the 54907 Eval Kit will work in that temperature range.

The Eval Kit has not been tested for this temperature range but the chip/module has been tested as noted in the datasheet.

0 Likes