- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
We bought the module with chip CYW43340 and hope to apply it in one large project.
I ported the WICED drivers for the CYW43340 with interface SDIO in my controller (Renesas with Cortex-M4 core 240 MHz).
Firmware for the module i took from WICED SDK 6.4 (Version: 6.49.29 (r714254) )
A RTOS ThreadX and their TCP stack run on my controller.
But I can’t get FTP transfer speed through the module more than 3 MByte/s on the 2.4 GHz band, and 5 MByte/s on the 5 GHz band.
Its not problem with TCP stack or SDIO interface, as I see long stall states from WiFi module side.
The transmission conditions were created perfect, the W-Fi router was 1 m from the module
Computer through the same router transmitted FTP data with a speed of more than 10 MByte/s
The question is whether the CYW43340 are capable of transmitting TCP data (in particular FTP) with a speed of more than 6 MByte/s
and whether exist evoluation board with this chip that could be connected to a PC to check the maximal speed?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello:
Would you please update the SDIO rate setting in your project ? and for this question:
The question is whether the CYW43340 are capable of transmitting TCP data (in particular FTP) with a speed of more than 6 MByte/s .
I can see the value in some cell phone project with high performance host core .
I will have a try on my 43340 evb.