Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
MiTo_1583836
Level 5
Level 5
50 likes received 25 likes received 10 likes received

I just went through the re-installation of SDK 3.7.0-3 on Mac OS X and came across few things that I would like to highlight in this post. It may be helpful for someone else.

The installation is performed on El Capitan: 10.11.6, the WICED SDK is downloaded from here: WICED Wi-Fi Documents & Downloadsselect a *.7z file, those are for Mac OS X.

The steps are:

  1. Run the instance of WICED Wi-Fi Eclipse CDT. If Eclipse is not installed yet: please use this one here: WICED-SDK-2.4.1 IDE & SDK [Mac OS X Package Installer]There is only one release of the Mac OS X Package installer so you have to start with this version even though the SDK is not the latest one!
  2. When Eclipse is up and running, do File->Import->Existing Project Into Workspace
  3. Under "Select root directory" select the decompressed *.7z SDK that you just downloaded above.
  4. Select "WICED-SDK-xxx" (for example: WICED-SDK-3.7.0-3) under Projects.
  5. Usually I would not select "Copy projects into workspace" (that's just my current configuration).
  6. Working sets not selected for this example.
  7. Press "Finish".
  8. You should see now under the imported project called WICED-SDK-xxxx (for example: WICED-SDK-3.7.0-3) under "Project Explorer".
  9. Also the "Make Target" window should be populated with the project.
  10. If you see folders and source code under the Make Target, just press the button called "Hide Empty Folder", this will keep the rules only (cleaner!).
  11. At this point you should see the build window with an error similar to the one below (see Logs of error during SDK install, Step 11 below)
  12. The make used to build is not the right one, you need to use the make provided with the SDK.
  13. Configure the proper make file via: Project->Properties->Builder, remove the check for "Use default build command", replace the make with: ${workspace_loc:/WICED-SDK-3.7.0-3}/make 
  14. Press Apply and close the window.
  15. Create a rule in the Make Target window as follow: snip.scan-BCM943362WCD4
  16. Execute the the build by clicking on the Target rule created above, see successful logs under STEP16 below

Logs of error during SDK install:

Step 11:

make all

tools/makefiles/wiced_toolchain_common.mk:202: *** incorrect 'make' used (/Applications/Xcode.app/Contents/Developer/usr/bin/make) - please use:  (Windows) .\make.exe <target_string>    (OS X, Linux) ./make <target_string>.  Stop.

STEP 16:

**** Build of configuration Default for project WICED-SDK-3.7.0-3 ****

/Users/mickael/Documents/WICED_WiFi/WICED-SDK-3.7.0-3/make snip.scan-BCM943362WCD4

MAKEFILE MAKECMDGOALS=snip.scan-BCM943362WCD4 OTA2_SUPPORT is disabled

Making config file for first time

+-----------------------------------------------------------------------------------------------------+

| IMPORTANT NOTES                                                                                     |

+-----------------------------------------------------------------------------------------------------+

| Wi-Fi MAC Address                                                                                   |

|    The target Wi-Fi MAC address is defined in <WICED-SDK>/generated_mac_address.txt                 |

|    Ensure each target device has a unique address.                                                  |

+-----------------------------------------------------------------------------------------------------+

| MCU & Wi-Fi Power Save                                                                              |

|    It is *critical* that applications using WICED Powersave API functions connect an accurate 32kHz |

|    reference clock to the sleep clock input pin of the WLAN chip. Please read the WICED Powersave   |

|    Application Note located in the documentation directory if you plan to use powersave features.   |

+-----------------------------------------------------------------------------------------------------+

MAKEFILE MAKECMDGOALS=snip.scan-BCM943362WCD4 OTA2_SUPPORT is disabled

Building Bootloader

Finished Building Bootloader

Processing resources

Creating security credentials

Making DCT image

Compiling App_Scan

Compiling Platform_BCM943362WCD4

Compiling WICED

Compiling Lib_SPI_Flash_Library_BCM943362WCD4

Compiling Lib_GPIO_button

Compiling WWD_ThreadX_Interface

Compiling WICED_ThreadX_Interface

Compiling WWD_for_SDIO_ThreadX

Compiling Supplicant_BESL

Compiling Lib_DNS

Compiling NetX_Duo

Compiling Lib_Wiced_RO_FS

Compiling STM32F2xx

Compiling Lib_TLV

Compiling Lib_base64

Compiling Lib_Linked_List

Compiling Lib_crypto_open

Compiling Lib_micro_ecc

Compiling WWD_NetX_Duo_Interface

Compiling WICED_NetX_Duo_Interface

Compiling common_GCC

Compiling STM32F2xx_Peripheral_Drivers

Compiling Lib_Ring_Buffer

Compiling Lib_crc

Compiling Lib_DHCP_Server

Compiling STM32F2xx_Peripheral_Libraries

Making build/snip.scan-BCM943362WCD4/libraries/App_Scan.a

Making build/snip.scan-BCM943362WCD4/libraries/Platform_BCM943362WCD4.a

Making build/snip.scan-BCM943362WCD4/libraries/WICED.a

Making build/snip.scan-BCM943362WCD4/libraries/Lib_SPI_Flash_Library_BCM943362WCD4.a

Making build/snip.scan-BCM943362WCD4/libraries/Lib_GPIO_button.a

Making build/snip.scan-BCM943362WCD4/libraries/WWD_ThreadX_Interface.a

Making build/snip.scan-BCM943362WCD4/libraries/WICED_ThreadX_Interface.a

Making build/snip.scan-BCM943362WCD4/libraries/WWD_for_SDIO_ThreadX.a

Making build/snip.scan-BCM943362WCD4/libraries/Supplicant_BESL.a

Making build/snip.scan-BCM943362WCD4/libraries/Lib_DNS.a

Making build/snip.scan-BCM943362WCD4/libraries/NetX_Duo.a

Making build/snip.scan-BCM943362WCD4/libraries/Lib_Wiced_RO_FS.a

Making build/snip.scan-BCM943362WCD4/libraries/STM32F2xx.a

Making build/snip.scan-BCM943362WCD4/libraries/Lib_TLV.a

Making build/snip.scan-BCM943362WCD4/libraries/Lib_base64.a

Making build/snip.scan-BCM943362WCD4/libraries/Lib_Linked_List.a

Making build/snip.scan-BCM943362WCD4/libraries/Lib_crypto_open.a

Making build/snip.scan-BCM943362WCD4/libraries/Lib_micro_ecc.a

Making build/snip.scan-BCM943362WCD4/libraries/WWD_NetX_Duo_Interface.a

Making build/snip.scan-BCM943362WCD4/libraries/WICED_NetX_Duo_Interface.a

Making build/snip.scan-BCM943362WCD4/libraries/common_GCC.a

Making build/snip.scan-BCM943362WCD4/libraries/STM32F2xx_Peripheral_Drivers.a

Making build/snip.scan-BCM943362WCD4/libraries/Lib_Ring_Buffer.a

Making build/snip.scan-BCM943362WCD4/libraries/Lib_crc.a

Making build/snip.scan-BCM943362WCD4/libraries/Lib_DHCP_Server.a

Making build/snip.scan-BCM943362WCD4/libraries/STM32F2xx_Peripheral_Libraries.a

Making snip.scan-BCM943362WCD4.elf

Making snip.scan-BCM943362WCD4.bin

snip.scan-BCM943362WCD4

----------------------------------|---------|---------|

                                  |         |  Static |

              Module              |  Flash  |   RAM   |

----------------------------------+---------+---------|

App                               |     404 |       0 |

crc                               |    1060 |       0 |

Host MCU-family library           |   13821 |    2737 |

Interrupt Vectors                 |     388 |       0 |

libc                              |   23551 |    3064 |

Networking                        |     989 |    8523 |

NetX-Duo - Interfaces & Stacks    |       0 |      16 |

Other                             |    3678 |      92 |

Packet Buffers                    |       0 |   23086 |

platform                          |    1024 |     168 |

RAM Initialisation                |    2316 |       0 |

resources                         |      16 |       0 |

Ring_Buffer                       |     116 |       0 |

Startup Stack & Link Script fill  |       9 |       3 |

ThreadX                           |    7868 |     396 |

TLV                               |      28 |       0 |

Wi-Fi Firmware                    |  210624 |       0 |

WICED                             |    3909 |     980 |

WWD                               |   14391 |    3007 |

----------------------------------+---------+---------|

TOTAL (bytes)                     |  281876 |   42072 |

----------------------------------|---------|---------|

Build complete

Making .gdbinit

0 Replies