WICED Studio 6.2.1
============================
Changes for WICED-SDK 6.2.1
===========================
* Applications
* Chip/Platform support
* Added support for Arrow QuickSilver EVK Platform (Murata 1GC/CYW43907 based).
* Added support for CYW943455EVB_02 (STM32H+43455) platform with the following features:
* BSP, peripheral drivers and IO applications based on FreeRTOS
* Middleware, Network stack and applications based on FreeRTOS and LWIP
* [4390x WiFi] Fixed issue of XIP mode unable to program large file (>1347584 bytes) in sflash.
* [STM32F4XX] Added SPI Slave driver support for STM32F4XX platform
* Support SPI active high chip select signal on STM32 platforms
* [4390x] Added FRAM support in 4390x sflash driver.
* [CY8CKIT_062] Updated Wiced CapSense Code to be Consistent to ES100 PDL and PSoC Creator generated CapSense files.
* Libraries, Protocols, Drivers
* [WICED pro 4390x] Enhancements to WICED audio and Apollo libraries:
* audio_render - adjusted late/early audio calculations
* 8021as/ascu - adjustments to wiced_time_read_8021as()
* Apollo - Enhanced to use BT embedded firmware by default on CYW20706A2 with CYW943907WAE4 platforms
* Apollo streamer - Added statistics and refined timestamping strategy
* audio_render - Improved silence insertion strategy
* Apollo - Changes to support IP multicast in addition to RMC
* Enabled support for TLS advanced security curves in AVS
* Added playback sample rate above 48kHz to CS47L24 codec
* Fixed playback state reporting to AVS library
* Gedday enhancements and fixes:
* Fixed DHCP thread stack corruption related to IPv6 AUTO IP
* Added fixes in Gedday for WICED to discover MDNS services
* Fixed MDNS record TTL values as per the RFC
* Remove PTR record and add cache flush bit for the records in MDNS update service advertisement sent during add/remove pairing
* Enchancements and fixes to HomeKit library:
* Added Secure WAC and Software Authentication support for IP and BLE transport. This is a preview version.
* Added support for uint64 and double data formats for HomeKit characteristic values
* Improved error handlings in HomeKit iCloud request processing
* Added fixes for HomeKit certification test case failures - TCC014, TCC028, TCH044.
* Removed "AUTO_IP_ENABLED" flag from the HomeKit library
* [WICED pro 4390x] Bluetooth audio hybrid mode support
* [CYW9MCU7X9N364] Gateway app cleanup
* [all WiFi] Upgraded mbedtls stack to version 2.6.0
* BLE WiFi Introducer app cleanup
* [all WiFi] Enhancements to FreeRTOS/LwIP:
* Upgraded to LwIP 2.0.3
* Modified auto IP handling in LwIP stack to pass BCT
* Added websocket library
* [all WiFi] Fixed enterprise security issue where WICED failed to associate to IAS server in PEAP
* [all WiFi] Verified enterprise security support with FreeRadius and IAS servers over EAP-TLS, EAP-TTLS and PEAPv0; including 802.11r and Fast Roaming
* [CYW94343x] Modified Bluetooth firmware with CoEx and throughput improvement fixes
* [all WiFi] BESL - Integrated uECC functions for ECC cipher operations in BESL instead of mbedTLS ECC for performance driven applications (can be configured by the application to pick uECC or mbedTLS-ECC)
* [all WiFi] Added support for AWS Greengrass connectivity. Unified AWS library for AWS IoT Cloud/Greengrass Core connections.
* [all WiFi] Upgraded cJSON library
* [4390x] Integrated hardware crypto engine with BESL/mbedtls - TLS funtionality on 4390x shall use hw crypto library by default
* [all WiFi] Enhancements and stability fixes to SSDP library
* Added OTA_SUPPORT flag in platform_config.h to enable OTA Support
* [all WiFi] Resolved memory leaks during long haul enterprise security join-leave tests
* [all WiFi] Added support to configure multiple certificate & key pairs for BESL TLS based servers
* [all WiFi] Added API to DNS library to provide a list of all resolved IP addresses
* [all WiFi] BESL - Improved TLS handshake timing for DHE cipher suite
* [CYW943907WAE4] Added support for Bluetooth Low Power Mode (LPM)
* Stability fixes to BTEWICED host stack including pairing fixes as central keyboard
* [all WiFi] Resolved stability issues with AMQP library
* [all WiFi] Incorporated Coverity fixes to several WICED components - supplicant, BESL, WiFi mesh, HTTP2, Gedday, WWD, Platform BSP drivers, MQTT, BTEWICED stack, AWS, OTA2, WICED Audio and WICED HCI BT library
* New WLAN firmware (7.45.98.50) added for 43364/43438/4343W platforms.
* Various Coverity fixes
* Coex fix for LE Connection getting lost with UDP Tx Traffic
* Enhanced Krack fix
* New WLAN firmware (7.15.168.114) added for 4390x/54907 platforms
* Fix Codenomicon test issues
* Fix CYW954097AEVAL1F 11AC certification test 5.2.27 issue
* Fix for low TCP Tx/Rx throughput with ACL
* Synchronize phy watchdog to data flow to avoid packet loss
* Fix Wiced errors setting up softap channel in 5G band
* New WLAN firmware (5.90.230.31) added for 43362 platforms
* Infrastructure
* Upgraded toolchain to GCC 7.2.1
Not able to install it on linux-64.
I'm sure I have enough free space, but it keep shows below dialog.
I've seen this issue before. Here's one example: WICED Studio 5.1 Install on Windows 7: Not enough free disk space , but I think there are others as well.
Please post a new discussion here: WICED Studio Wi-Fi/Combo Forums and someone from the AE team will help you debug the install.
mifo wrote:
Please post a new discussion here: WICED Studio Wi-Fi/Combo Forums and someone from the AE team will help you debug the install.
I just posted new discussion with some of my comments. Hope to get the fix soon.
Thanks.
When can we see Ariplay 2 support?
Cannot install WICED Studio 6.2.
My username contains a language specific character ("ö") which is not accepted by the installer. Is there a way to change the user path? Changing the installation path does not work.
Bob
PS: I am not willing to create a new user on my PC just for WICED work.
Not sure, but perhaps this workaround will resolve the special character issue: Install problems related to white space in path - WICED Studio 5.x
If not, please post a new discussion here: WICED Studio Wi-Fi/Combo Forums and someone from the AE team will help you debug the install.