Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Wi-Fi Combo Forum Discussions

user_2199751
Level 2
Level 2
First like given

We are currently developing a product using SPIL BCM4390 based module, SB-WM-N03. However, we found that the EVB boards we have cannot associate AP properly. We have tried both with 3.1.2 SDK and 3.3.1 however, both showed failures.

We also tried with BCM43362 module and it worked OK.  We tested this with IP time AP without Security enabled.

If we turned this to AP mode, it works OK.

I am wondering if there is anyone experienced this issue before.  It seems that the issue is very basic functionality.

Hope to have some clarification from BRCM.

Thanks

Won

0 Likes
14 Replies
Anonymous
Not applicable

With both 3.1.2 and 3.3.1, the BCM4390 works fine to associate AP for us.

Did you test it with snip code?

Maybe you need to describe more detail about how you test it.

0 Likes

Hi Sam,

Thanks for your comment.

Yes, we used snip code.

We will share more details as we try to gather more data point.

What we just found out that it works when the AP is set to 11b/g mode but it does not work when it is set to 11/b/g/n mixed mode.

AP information

IPtime AP N704-0v3

Settings

Channel Bandwidth: 20/40MH

Long preamble

Channel: Channel 1

Security: Open

Mode: B,G,N mixed

Thanks

Won

0 Likes
Anonymous
Not applicable

Does it work if you set your AP to 20MHZ only?

In our test, BCM4390 does not work with 20/40 Mix (or Auto) case.

I'm also confused why it does not work in 20/40 Mix.

BTW, can you confirm again if BCM43362 works with 20/40 Mix case?

I want to know if the 20/40 Mix isssue is BCM4390 only or not.

Thanks.

0 Likes
Anonymous
Not applicable

Hi,

I just did the "20/40 mixed" test on both BCM43362 and BCM4390 myself and

found BCM43362 works but BCM4390 does not work.

So can someone help to fix the "20/40 mixed" for BCM4390?

Note, I test on both sdk-3.1.2 and sdk-3.3.1 and get the same result.

0 Likes

Hi Sam,

Thanks for your comment.

As you commented, our test also showed this mixed mode failure.

We contacted our disty and asked for an official FW fix for this issue.

Perhaps, you can do the same to your disty folks.

Best Regards

Won

0 Likes
Anonymous
Not applicable

Hi,

We have contacted the disty for this issue but still don't get the fix so far.

As far as I know, obewen already got the fix, which means the

fix is available.

Can someone help?

Thanks.

0 Likes
Anonymous
Not applicable

Sam:

   We have worked with Broadcom to get the patch via disty channel, and will release to you soon.

0 Likes
Anonymous
Not applicable

BCM4390 4390 has problem with HT40 mixed mode.

It will be ok soon.

0 Likes

How long is "soon"? We are experiencing the same problem here and it is obviously a roadblock for us.

Thanks,

Fredrik

0 Likes
Anonymous
Not applicable

Hi Fredrik,

I've checked with the software team and am advised that SDK3.3.1 has all the current fixes integrated.  Can you please retest with 3.3.1 and advise if you still see this issue.

Regards

Dave

0 Likes
Anonymous
Not applicable

We are using SDK3.3.1 and see the same issue when 40MHz is enabled. Does the newer version of SDK resolve this?

0 Likes
Anonymous
Not applicable

Hello Lakshmi,

We do not support 40MHz operation in the 2.4GHz band as this is not required for Wi-Fi Alliance interoperability certification.

Regards
Dave

0 Likes
Anonymous
Not applicable

What I meant is that if the AP is set up for mixed mode (20/40MHz), it does not work. If we change it to 20MHz only, 4390 can connect to it.  We are using SDK 3.3.1.

0 Likes
Anonymous
Not applicable

It should work if you use 3.4.0+ SDK.

0 Likes