I need an example or documentation on implementing a USB slave device on STM32F4. We are using WICED and ThreadX.
We are using our own board.
Solved! Go to Solution.
Hi @jdreitzler ,
Below attached the link which has details how to configure CYW943907AEVAL1F as USB device. You can take this as reference to use USB in your board.
Thanks,
Rakesh B G
Hi @jdreitzler ,
Below attached the link which has details how to configure CYW943907AEVAL1F as USB device. You can take this as reference to use USB in your board.
Thanks,
Rakesh B G
Above link has a note:
The USB Device functionality does not work for device classes (For instance, mass storage class) that use a transfer data length which is a multiple of the maximum packet size. Currently there is no workaround for this issue. The issue is being investigated and will be updated once there is a solution or workaround identified.
That link was posted on 2017, I'm wondering if "transfer data length with multiple of the maximum packet size" is still an issue or not with wiced-6.6.1?
Is there an example that is not HID? We have a serial port CLI that we want to port to USB. So I'm guessing we need a USB device class...not HID...
Hi @jdreitzler ,
Unfortunately In wiced, we don't have an example code other than HID.
Thanks,
Rakesh B G