- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
From the two modules that I have of CYW954907EVAL-1F, I want one of my boards configured as STA to connect to an AP. While referring to the API reference guide, I came across the function "wwd_wifi_join". The same is declared as follows:
wwd_result_t wwd_wifi_join ( const wiced_ssid_t ∗ ssid, wiced_security_t auth_type, const uint8_t ∗ security_key, uint8_t key_length, host_semaphore_type_t ∗ semaphore, wwd_interface_t interface )
I have defined following parameters in my AP:
- SSID = 802.11ac_try1
- Authentication type = WICED_SECURITY_WPA2_AES_PSK
- Security key = 80211AC
- Key Length = The length of the Security key in bytes
My questions are as follows:
- How would I calculate the security key length in bytes?
- What will be the interface in the function? Will it be WICED_AP_INTERFACE or WICED_STA_INTERFACE?
- In the module that has been configured as STA, how would I pass these parameters to the variables defined in the function so that it can join the SSID 802.11ac_try1.
- Not sure of how to use semaphore here? can anyone please throw some light?
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello HaTr_4568521
How would I calculate the security key length in bytes?
--> This will be given by "sizeof(your_passphrase) - 1". The -1 is to remove the "\0" at the end.
What will be the interface in the function? Will it be WICED_AP_INTERFACE or WICED_STA_INTERFACE?
--> The WICED_AP_INTERFACE is used when you are trying to setup the device as an AP and are trying to connect to the AP from other devices(clients). The WICED_STA_INTERFACE is used when you want to configure the device to act as a station(client) and want it to connect to an access point. Now since you are using the wwd_wifi_join() which is a driver level API to join an access point, the interface would be WICED_STA_INTERFACE.
Not sure of how to use semaphore here? can anyone please throw some light?
--> Can you throw some insight as to why you are in need of a semaphore for a join operation? Anyway the API explanations are available at /43xxx_Wi-Fi/doc/API/group__semaphores.html
In the module that has been configured as STA, how would I pass these parameters to the variables defined in the function so that it can join the SSID 802.11ac_try1
In this case since you are using the driver level API's, please refer to /43xxx_Wi-Fi/apps/wwd/ping to learn how to pass parameters.
Also, if you are just starting out, it would be better to start with WICED API's, Please refer to /43xxx_Wi-Fi/apps/snip/apsta as a starting point.
Thanks
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello HaTr_4568521
How would I calculate the security key length in bytes?
--> This will be given by "sizeof(your_passphrase) - 1". The -1 is to remove the "\0" at the end.
What will be the interface in the function? Will it be WICED_AP_INTERFACE or WICED_STA_INTERFACE?
--> The WICED_AP_INTERFACE is used when you are trying to setup the device as an AP and are trying to connect to the AP from other devices(clients). The WICED_STA_INTERFACE is used when you want to configure the device to act as a station(client) and want it to connect to an access point. Now since you are using the wwd_wifi_join() which is a driver level API to join an access point, the interface would be WICED_STA_INTERFACE.
Not sure of how to use semaphore here? can anyone please throw some light?
--> Can you throw some insight as to why you are in need of a semaphore for a join operation? Anyway the API explanations are available at /43xxx_Wi-Fi/doc/API/group__semaphores.html
In the module that has been configured as STA, how would I pass these parameters to the variables defined in the function so that it can join the SSID 802.11ac_try1
In this case since you are using the driver level API's, please refer to /43xxx_Wi-Fi/apps/wwd/ping to learn how to pass parameters.
Also, if you are just starting out, it would be better to start with WICED API's, Please refer to /43xxx_Wi-Fi/apps/snip/apsta as a starting point.
Thanks