cancel
Showing results for 
Search instead for 
Did you mean: 

Wi-Fi Combo

grphc_1578046
New Contributor II

This is follow up from the earlier EAP/PEAP debug sessions

Occurs every time.

When in local processor memory the connections do not fail.

The error is 1006.

  RESULT_ENUM( prefix, NOT_AUTHENTICATED, 1006 ), /**< Not authenticated */

0 Likes
1 Solution
GauravS_31
Moderator
Moderator

You will need to check how much memory is consumed in external flash during the enterprise join process. Alternately you can adjust the tunables such as packet pool size (TX_PACKET_POOL_SIZE and RX_PACKET_POOL_SIZE), disable iperf (CONSOLE_NO_IPERF), P2P (CONSOLE_NO_P2P) in console.mk. Please refer to doc/WICED-Enterprise-Security-User-Guide.pdf for more details. For further debugging, you can enable the supplicant macros (WPRINT_ENABLE_SUPPLICANT_DEBUG, WPRINT_ENABLE_SUPPLICANT_INFO, WPRINT_ENABLE_SUPPLICANT_ERROR) in wiced_defaults.h and mbedtls logs as explained in Debugging TLS in WICED

View solution in original post

2 Replies