Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Hi,

I was wondering if it would be possible to have more than one ( in my case, two ) pass phrases for the WPA authentication on the soft ap.

( or the p2p ).

I'm exploring the option of having two pass-phrases:

one would be a default hard-coded pass-phrase ( which would be a long random set of characters printed on the back of the device ), and the other is user-configurable.

I was thinking about adding a button for that purpose, but that has some additional remifications ( pcb layout, usability, cost, etc ).

btw : in 3.3.1 you've done a great job with extracting the function wwd_wifi_set_passphrase outside.. but you could get an extra bonus by using it in wiced_p2p.c:610.

Tsachi

0 Likes
1 Reply
Anonymous
Not applicable

bumping up, in case someone would know the answer.. ( which is likely to be "no" )

0 Likes