Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Wi-Fi Combo Forum Discussions

Anonymous
Not applicable

My application uses wiced_tcp_server_start() to implement a tcp server.

When test build with NetX/NetX_Duo, wiced_tcp_server_start() call in

my tcp server always return WICED_ERROR.

I found if I comment out the code to start http server, then my tcp server runs well.

If I run my tcp server earlier, then http server will fail at wiced_tcp_server_start().

The http server also use wiced_tcp_server_start(), so

It looks like wiced_tcp_server_start() can only be called once on NetX/NetX_Duo.

This issues does not happen on FreeRTOS+LwIP.

0 Likes
5 Replies
GregG_16
Employee
Employee
25 sign-ins 25 comments on KBA 10 comments on KBA

Just want to confirm, this is being done on different ports?  Correct?

0 Likes
Anonymous
Not applicable

Yes, it's listen on different port ( port 23).

I think it's very easy to test it by:

1. download the test_server.c from http://community.broadcom.com/thread/2561?sr=stream&ru=2286

2. Modify the test_server.c and add printing the return value of wiced_tcp_server_start()

   You might also want to print the return value of wiced_tcp_server_start() in http daemon.

3. Add the test_server.c code to apps/snip/ping_webserver

4. put start_test_server() before/after calling wiced_http_server_start().

   Then you can see either start_test_server() fails or wiced_http_server_start() fails

   at wiced_tcp_server_start() call. (depends on which one is called first.)

0 Likes
Anonymous
Not applicable

hi,

Just want to know if this bug will be fixed in sdk-3.1.1?

For NetX/NetX_Duo build:

The bug is that the second wiced_tcp_server_start() call always fail.

So I cannot use wiced_tcp_server_start() to implement tcp server because

http server uses wiced_tcp_server_start() already.

This is 100% reproducable.

I found yet another issue with LwIP build:

The second wiced_tcp_server_start() works in LwIP, so I have my tcp server

running. However, I found if I use browser to connect to the web page, then

my tcp server can only accept 1 client. the second client always fails.

If I try to connect my tcp server first, I can have 5 clients.

However, then http server has no response (and one of the client will be

disconnected automatically , probably due to the http request).

0 Likes
Anonymous
Not applicable

I found yet another issue with LwIP build:

The second wiced_tcp_server_start() works in LwIP, so I have my tcp server

running. However, I found if I use browser to connect to the web page, then

my tcp server can only accept 1 client. the second client always fails.

If I try to connect my tcp server first, I can have 5 clients.

However, then http server has no response (and one of the client will be

disconnected automatically , probably due to the http request).

My understanding of this problem is:

The system has a limitation for the number of tcp socket can be created at

the same time.

A wiced_tcp_server_start() may create at most 5 tcp sockets at the same time.

However, we don't know how many tcp sockets are created by a http server.

While using wiced_tcp_server_start() for other tcp server, it may fail to

to create socket because of reaching system limitation.

So if my tcp server create 5 tcp socket and keep the connection alive, it's

possible http_server always fails to create tcp socket and thus no response.

Currently the number of tcp socket can be created at the same time is a very

small number. And I have asked a question that is this configurable, but still

don't get a correct answer.

I tried increase WICED_DEFAULT_TCP_LISTEN_QUEUE_SIZE,

WICED_MAXIMUM_NUMBER_OF_ACCEPT_SOCKETS, and

WICED_MAXIMUM_NUMBER_OF_SOCKETS_WITH_CALLBACKS, but it does not work.

Yet another issue I have reported is that once reach the maximum number of

tcp socket can be created [1], I'm not able to create any tcp socket anymore.

As a result, either my tcp server always fails or the http_server always no

response.

Can someone help on this?

[1] http://community.broadcom.com/message/7080#7080

Anonymous
Not applicable

I also have similar issues. I am suing STA and AP interface and use TCP Server for each interface.

1. In  demo.s2w-BCM943362WCD4_DAMOSYS NO_BUILD_BOOTLOADER=1 download run

    it might be "ThredX + NetX"

  if I call "wiced_tcp_server_start" for STA interface then it works.

and another    call "wiced_tcp_server_start" for AO interface then it fails

    But in FreeRTOS+LwIP ,    Both works fine.