Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Wi-Fi Combo Forum Discussions

This widget could not be displayed.
Anonymous
Not applicable

Hi,

we are searching for a chip/solution to build up a large-scale 802.11s mesh network.

It is going to be used as a backbone for a control application to connect multiple 802.15.4 networks. Therefore, a 5 GHz solution would be preferred.

On the software side we would either use Linux (with the potential time-consuming task of writing a kernel driver for the chip) or an existing stack with 802.11s support (WICED?).

Any suggestions?

Greetings,

Florian

0 Likes
4 Replies
GregG_16
Employee
Employee
25 sign-ins 25 comments on KBA 10 comments on KBA

Since WICED is targeted for IoT applications so 5GHz is not typically needed.  I will have to see where we stand on any type of mesh support,

0 Likes

Any new news on 802.11s mesh support for the WICED stack?  We too would like to implement it in our solution.

0 Likes

Any news on mesh support for WiFi?

0 Likes

Nothing new at this time.  We will keep you posted if we hear anything.

0 Likes
This widget could not be displayed.