Schematic of BCM943362 WCD_EVB

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Hi,

I am using BCM943362WCD4_EVB base board with p100 label. I need the exact schematic for this base board.

The closest one is /platform/evaluation_boards/BCMWCD1EVAL/schematic/BCM9WCDEVAL_p400 based on the board front picture. However, the red top module is not the same in the above picture. My red module is BCM943362WCD with p200 label.

Please point me to the exact schematic drawing of the base board.

Thanks

NK

0 Likes
6 Replies
lock attach
Attachments are accessible only for community members.
GregG_16
Employee
Employee
50 sign-ins 25 sign-ins 25 comments on KBA

I believe this is what you need?

Anonymous
Not applicable

Thanks Gangi,

So this BCM9WCD1EVAL1_p405 is the schematic of BCM943362WCD4_EVB base board with p100 label?

Since the names don't match I just want to make sure.

Thanks

~NK

0 Likes

Here is the change log and the p100 Initial schematics.  Not sure if these effect you or not.

P405

Removed BCM94319WICED5 (100-122740-0000) from BOM of BCM9WCD1EVAL1 (100-120515-0000 ), taking BCM9WCD1EVAL1 to revision P405. BCM94319WICED5 was mistakenly added to the P403 BOM

P404

To add a USB cable to the top level assembly

P403

Populate BCM94319WICED5 module (This was a mistake and corrected in P405).

P402

Updated Quad AND gate to correct voltage rating

P401

Set the module (U1) to DEPOP to allow for hand assemble of other module variants

P400

Fixed reset bug, added expansion board to replace Canary

P300

Replaced analog switches with AND gates. Added BULK bypass cap. Removed usbpwren PFET

P200

Fixed Jlink selection, added led indicators

P100

Initial Release

0 Likes
lock attach
Attachments are accessible only for community members.

Here is the change log and the p100 Initial schematics.  Not sure if these effect you or not:

P405

Removed BCM94319WICED5 (100-122740-0000) from BOM of BCM9WCD1EVAL1 (100-120515-0000 ), taking BCM9WCD1EVAL1 to revision P405. BCM94319WICED5 was mistakenly added to the P403 BOM

P404

To add a USB cable to the top level assembly

P403

Populate BCM94319WICED5 module (This was a mistake and corrected in P405).

P402

Updated Quad AND gate to correct voltage rating

P401

Set the module (U1) to DEPOP to allow for hand assemble of other module variants

P400

Fixed reset bug, added expansion board to replace Canary

P300

Replaced analog switches with AND gates. Added BULK bypass cap. Removed usbpwren PFET

P200

Fixed Jlink selection, added led indicators

P100

Initial Release

0 Likes
Anonymous
Not applicable

Thanks Gangi.

Can I ask for a recent WICED WiFi board free of charge?

Regards

NK

On Jul 24, 2015 9:49 AM, "gangi" <communities-list@community.broadcom.com>

0 Likes
lock attach
Attachments are accessible only for community members.
Anonymous
Not applicable

Dear Gangi,

Both schematics don't match my base board. Please note the baseboard says

BCM943362WCD4_EVB P100.

I have attached the front and back pictures. Please send the correct

schematic. The footprint of the elements on the layout will be great if you

can provide that too.

Kind regards,

Nader

Nader Kalantari, PhD

Founder & CEO

ArianRF Inc.

Email: nader@arianrf.com

Phone: (949) 246 0848

0 Likes