- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
i have stm32f407 discovery board which is same as a STM32f417..
also one EVB which is with CYW43455.. same as like LSR-LWB 4343 board.
i'm using LSR-lwb 4343 platform file and "CYW943455EVB_02" platform file for make my own platform file.
i want to platform file for this setup. can you help me pls.?
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
You can refer to the STM32F469 porting in WICED to understand the platform organization in WICED Studio. Your idea of combining both of the platforms are correct.
On a very High level, source files for the host side (STM32F4xx) are mostly in platform.c, platform.h, platform_config.h which can be re-used from LSR-LWB 4343 and then comes the platform.mk file which needs to be modified with the makefile from CYW943455EVB_02.
NVRAM file (wifi_nvram_image) can be re-used from CYW943455EVB_02 for testing purposes.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
You can refer to the STM32F469 porting in WICED to understand the platform organization in WICED Studio. Your idea of combining both of the platforms are correct.
On a very High level, source files for the host side (STM32F4xx) are mostly in platform.c, platform.h, platform_config.h which can be re-used from LSR-LWB 4343 and then comes the platform.mk file which needs to be modified with the makefile from CYW943455EVB_02.
NVRAM file (wifi_nvram_image) can be re-used from CYW943455EVB_02 for testing purposes.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
it's really useful for me thanks
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Wiced is missing “WICED/WWD/internal/chips/43455/wwd_ap.c", is your problem solved?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
CYW43455 is not supported in WICED; only supported for Linux hosts. Hence, you don't see those files in WICED (earlier response is not perfectly valid anymore).