SSBWMN01 WICED Wi-Fi module platform file for WICED SDK 3.1.2.
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
Dear all,

Attachment is platform file for SSBWMN01 WICED Wi-Fi module which for WICED SDK 3.1.2.

FYI

Eugene

0 Likes
2 Replies
SeyhanA_31
Employee
Employee
250 replies posted 100 replies posted 50 replies posted

Thanks for sharing.

Seyhan

0 Likes
Sharn_Lin
Level 2
Level 2
10 sign-ins 5 questions asked 5 sign-ins

Hi Eugene,

When I tried gpio example, the LEDs never flash, it seems something wrong on LED definition

platform.h

gpio_err.png

#define WICED_LED1       (WICED_GPIO_17)

#define WICED_LED2       (WICED_GPIO_18)

I check the schematic of SSBWMN01, that the LEDs are connect to MICRO_GPIO_0/1 but the pin of N01 should be 62/63 not 45/46 as above.

after change LEDs define from WICED_GPIO_17/18 to WICED_GPIO_28/29, the LEDs works well.

Do you have the latest platform files, I am not sure if any other thing I missing.

Best regards,

Sharn

0 Likes