Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Wi-Fi Combo Forum Discussions

This widget could not be displayed.
Anonymous
Not applicable

I used to flash my STM32F429 discovery board using Jlink base JTAG programmer, anyway after many code flashing and reflashing Now when I try to debug my program ,when I click the Start/Resume button I receive a SIGINT interrupt can't go further debugging.

Also if I use "snip.sntp_get_time-STDiscovery429_BCM43362-FreeRTOS-LwIP-SDIO JTAG=jlink-debug download"

IDE fails to program the device ,but If I use just "download run"I can flash the device.

What might be causing this issue to happen ?

hh.jpg

Also Once I flash the code to board I have to power cycle it to get the new code running ,

Is this some kind of IDE bug or have I messed up the hardware?

0 Likes
1 Reply
SeyhanA_31
Employee
Employee
100 likes received 50 likes received 25 likes received

Hi,

I tried using Olimex ARM-USB-TINY-H and it works as expected with Make Target "snip.scan-STDiscovery429_BCM43362-debug JTAG=Olimex_ARM-USB-TINY-H download run".

Try "snip.sntp_get_time-STDiscovery429_BCM43362-FreeRTOS-LwIP-SDIO-debug JTAG=jlink download".

Seyhan

0 Likes
This widget could not be displayed.