- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
rroy
Per our previous closed discussion here: CYW43907 SDIO Slave
Is it possible to receive 43907 Programmers Guide, and Register Map/Definitions with NDA agreement to implement SDIO slave by myself?
I try to implement driver by pieces of info in library, but get stuck in several things.
I`ve defined some structures for SDIO device (as analog of sdioh_info_t) and start to initialize structures like in sdioh_attach in bcmsdstd.c
I have add info to core info
{
.curmap = (void*)PLATFORM_SDIOD_REGBASE(0x0),
.curwrap = (void*)PLATFORM_SDIOD_MASTER_WRAPPER_REGBASE(0x0),
.coreid = SDIOD_CORE_ID,
.corerev = SDIOD_CORE_REV,
},
then Ive copy some function for reading and writing registers.
static uint8 read_sdiod_reg8(sdio_device_info_t *sd, uint reg)
{
volatile uint8 data = *(volatile uint8 *) (sd->mem_space + reg);
dsd_ctrl(("8: R Reg 0x%02x, Data 0x%x\n", reg, data));
return data;
}
static void write_sdiod_reg8(sdio_device_info_t *sd, uint reg, uint8 data)
{
*(volatile uint8 *)(sd->mem_space + reg) = (uint8) data;
dsd_ctrl(("8: W Reg 0x%02x, Data 0x%x\n", reg, data));
}
Then I`ve implement function for os allocation and free (sdiod_mos_init,sdiod_mos_free) and try to read and write registers, defined in sdio.h
void application_start(void)
{
wiced_init();
sdiod_init(0);
while(1)
{
printf("hi\r\n");
wiced_rtos_delay_milliseconds(10000);
}
}
int sdiod_init( void *cb_func)
{
sdio_device_info_t *dsd;
dsd_trace(("%s\n", __FUNCTION__));
if ((dsd = (sdio_device_info_t *) malloc(sizeof(sdio_device_info_t))) == 0){
dsd_err(("sdioh_attach: out of memory, malloced %d bytes\n", MALLOCED(0)));
return 0;
}
memset((char*)dsd,0, sizeof(sdio_device_info_t));
sdiod_mos_init(dsd);
osl_core_enable(SDIOD_CORE_ID);
dsd->mem_space = (volatile char *)PLATFORM_SDIOD_REGBASE(0x0);
if (dsd->mem_space == NULL) {
dsd_err(("%s:ioremap() failed\n", __FUNCTION__));
sdiod_mos_free(dsd);
free(dsd);
}
if(cb_func != NULL) {
dsd->intr_handler = cb_func;
dsd->intr_handler_arg = NULL;
dsd->intr_handler_valid = TRUE;
} else {
dsd->intr_handler = NULL;
dsd->intr_handler_arg = NULL;
dsd->intr_handler_valid = FALSE;
}
read_sdiod_reg8(dsd, SDIOD_CCCR_REV);
read_sdiod_reg8(dsd, SDIOD_CCCR_SDREV);
read_sdiod_reg8(dsd, SDIOD_CCCR_IOEN);
write_sdiod_reg8(dsd,SDIOD_CCCR_IOEN,SDIO_FUNC_ENABLE_1|SDIO_FUNC_ENABLE_2|SDIO_FUNC_ENABLE_3);
read_sdiod_reg8(dsd, SDIOD_CCCR_IOEN);
read_sdiod_reg8(dsd, SDIOD_CCCR_IORDY);
read_sdiod_reg8(dsd, SDIOD_CCCR_INTEN);
read_sdiod_reg8(dsd, SDIOD_CCCR_INTPEND);
read_sdiod_reg8(dsd, SDIOD_CCCR_IOABORT);
read_sdiod_reg8(dsd, SDIOD_CCCR_BICTRL);
read_sdiod_reg8(dsd, SDIOD_CCCR_CISPTR_0);
}
At all CYW43907 have error while reading SDIOD_CCCR_CISPTR_0, and SDIOD_CCCR_IOEN didnt write a parameters.
So, it`s nessesary for me to receive your guides to proceed my work, cause now I didn`t know what bus clocks I`ve missed to initialize or which register have R R/W W attributes etc....
Thanks a lot for replies!
Solved! Go to Solution.
- Labels:
-
ispn:36623:1:0
-
l1:3966:1:0
-
l2:6066:1:0
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Please contact Cypress sales and explain your requirements. We do not disclose this document in community.