Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
iono_4292956
Level 1
Level 1
First like given

Hi,

I have two question:

a) Any way in WICED SDK to sign the image file : elf or bin. I have reuiqrment from client to sign image, so looking for solution.

b) WICED makes .elf and use openocd to flash. Also makes .bin file. Any way to use .bin to flash? I tried openocd command:

flash write_image erase my_bin.bin 0x08000000

0x08000000 is stm32 flash start location. But cannot boot after flash. I think all placement/padding information lost. Can you help?

0 Likes
3 Replies
Aditi_B
Moderator
Moderator
Moderator
500 replies posted 5 questions asked 250 replies posted

Hi,

Have you tried the openocd command mentioned in the following link to write .bin to flash?

Re: How do I write a binary image to WICED micro?

Let us know if you face any issues.

Thanks

My openocd command is same. I remove extra config file to keep simple for my question.

I think i know problem. linker app code location is at 0x0800C000 because space reserved for bootloader and dct, so I cannot flash app code at 0x08000000. I have one follow up question. This is linker file:

MEMORY

{

    BTLDR_VECTORS    (rx)  : ORIGIN = 0x08000000, LENGTH = 512

    SHARED_API       (rx)  : ORIGIN = 0x08000200, LENGTH = 512

    BTLDR_CODE       (rx)  : ORIGIN = 0x08000400, LENGTH = 15K

    DCT1_FLASH       (rx)  : ORIGIN = 0x08004000, LENGTH = 16K

    DCT2_FLASH       (rx)  : ORIGIN = 0x08008000, LENGTH = 16K

    APP_CODE         (rx)  : ORIGIN = 0x0800C000, LENGTH = 976K

    SRAM             (rwx) : ORIGIN = 0x20000000, LENGTH = 256K

    BTLDR_SRAM       (rwx) : ORIGIN = 0x2001BC00, LENGTH = 17k       /* Boot loader stack at the end. */

}

I can flash app code at 0x0800C000 correctly.

Please tell me if I use bootloader.bin(waf.bootloader-NoOS) and flash at 0x08000000, it will take care of BTLDR_VECTORS, SHARED_API, BTLDR_CODE?

Do I need to flash DCT at DCT1_FLASH and DCT2_FLASH two time? I am not sure what the .elf version will do?

May be it is better idea to combine all separate .bin (bootloader + dct.bin + app.bin) into one .bin file for flashing. Any idea to combine correctly?

Also, please help with image sign question.

0 Likes

Hi,

I find "ota2_manuf_image" target use perl script to comine binary. Is it made for one flash memory (internal or external)? In my examply, I have no OTA2, but OTA1, so I use internal flash and external flash . Will script create one binary for both flash that can be use by openocd???

0 Likes