- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I have a question regarding with STM32F4DIS-WIFI Module(Murata SN8200). I need to connect the RTS\CTS pins to make the handshaking between the module and the Microprocessor board. Any idea about how to do that using the WICED, and how can I download the code on the module or embed it in the firmware?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
Moved your question to Murata's space.
Seyhan
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I couldn't find the answer for my question!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
This blog How to Enable UART2 on BCM943341 EVB show how to setup another UART (UART2) for different MCU but setup is similar for your MCU as well.
For each UART setup CTS and RTS signals could be defined as well. Replace the following null definitions for CTS and RTS
.cts_pin = NULL,
.rts_pin = NULL,
with mapped CTS and RTS pin definitions in "const platform_uart_t platform_uart_peripherals[] =" located in your platform file, \platforms\SN8200x\platform.c.
Below is the example of CTS and RTS definitions for BCM43341 for UART2:
.cts_pin = &platform_gpio_pins[WICED_GPIO_15],
.rts_pin = &platform_gpio_pins[WICED_GPIO_16],
Seyhan
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi seyhan,
I am Using BCM-943362 Board. Simple Rx and Tx is working fine.
I wanted the flow control for the UART (RTS/CTS).
How do I Defined it. ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
Try adding following to "const platform_uart_t platform_uart_peripherals[]=" definition in platforms/BCM943362WCD4/platform.c platform definition file.
[WICED_UART_2] =
{
.port = USART2,
.tx_pin = &platform_gpio_pins[WICED_GPIO_3],
.rx_pin = &platform_gpio_pins[WICED_GPIO_4],
.cts_pin = &platform_gpio_pins[WICED_GPIO_1],
.rts_pin = &platform_gpio_pins[WICED_GPIO_2],
.tx_dma_config =
{
.controller = DMA1,
.stream = DMA1_Stream6,
.channel = DMA_Channel_4,
.irq_vector = DMA1_Stream6_IRQn,
.complete_flags = DMA_HISR_TCIF6,
.error_flags = ( DMA_HISR_TEIF6 | DMA_HISR_FEIF6 ),
},
.rx_dma_config =
{
.controller = DMA1,
.stream = DMA1_Stream5,
.channel = DMA_Channel_4,
.irq_vector = DMA1_Stream5_IRQn,
.complete_flags = DMA_HISR_TCIF5,
.error_flags = ( DMA_HISR_TEIF5 | DMA_HISR_FEIF5 | DMA_HISR_DMEIF5 ),
},
},
USART2 pins on the BCM943362WCD4 EVB are routed to J7 header.
PA0 CTS -> J7-9
PA1 RTS -> J7-3
PA2 Tx -> J7-4
PA3 Rx -> J7-5
Seyhan
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
seyhan
In my code for UART I am doin as below.
char startCmd2[20] = {0x02,0x01,0x02,0x08,0x08,0x02,0x02,0x56,0x65,0x15,0x45,0x65,0x98,0x12,0x32,0x45,0x12,0x46,0x23,0x32};//0x02,0x01,0x02,0x08,0x08};
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi seyhan.
In my code for UART I am doin as below.
char startCmd2[20] = {0x02,0x01,0x02,0x08,0x08,0x02,0x02,0x56,0x65,0x15,0x45,0x65,0x98,0x12,0x32,0x45,0x12,0x46,0x23,0x32};//0x02,0x01,0x02,0x08,0x08};
char recvData[20];
memset(recvData,0, (sizeof(recvData)/sizeof(recvData[0])));
wiced_init();
wiced_gpio_output_high( WICED_LED1 );
// checking the UART for REsult
wiced_result_t result;
/* Initialise ring buffer */
ring_buffer_init(&rx_buffer, rx_data, RX_BUFFER_SIZE );
/* Initialise UART. A ring buffer is used to hold received characters */
wiced_uart_init( STDIO_UART, &uart_config, &rx_buffer );
/* Send a test string to the terminal */
wiced_uart_transmit_bytes( STDIO_UART, TEST_STR, sizeof( TEST_STR ) - 1 );
for(loopCnt=0; loopCnt<=(sizeof(startBleCmd2)/sizeof(startBleCmd2[0])); loopCnt++)
{
wiced_uart_transmit_bytes( STDIO_UART, &startBleCmd2[loopCnt], 1);
}
memset(startBleCmd2,0, (sizeof(startBleCmd2)/sizeof(startBleCmd2[20])));
while(1)
{
if(wiced_uart_receive_bytes(STDIO_UART, recvData, sizeof(recvData), WICED_NEVER_TIMEOUT ) == WICED_SUCCESS )
/* De-Initialization of UART*/
wiced_uart_deinit(STDIO_UART);
}
My question is , I am Able to send the data over UART to another Controller. But when I check There its showing garbage values there.
As In my buffer if i am sending 0x02 as first byte, On another Controller it's showing garbage.
Need guidance In this issue.
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
Have you disabled STDIO?
You are using the same UART so you need to make sure that STDIO is disabled in the makefile
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
And make sure that you have enabled RTS_CTS flow control in the uart configuration parameter
Look at the BCM94343WWCD1 platform files on how to do this
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
If you are interested to know. The NXP kit, OM13086, is powered by ZentriOS and uses the Murata SN8200 module.
here is a direct link: http://www.nxp.com/products/identification-and-security/authentication/lpc43s67-a70cm-cloud-connecti...
LPC43S67-A70CM Cloud Connectivity Kit|NXP
See ZentriOS running on the Murata SN8xxx and NXP LPC Microcontroller