Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
NiMc_1688136
Level 5
Level 5
10 sign-ins 50 questions asked 10 solutions authored

During a battery discharge test, we let our product discharge until the battery cut off. At the moment we believe there is a hw issue with our battery controller that allows the battery to connecting and disconnecting as a source when it is at a low threshold but that is a different issue. During this rebounding behavior of the battery, i managed to catch one device entering a watchdog timeout in app code, somewhere in the wiced_init function. These watchdogs appears to have forced a factory image rollback. At this point, 3 of the devices would not recover with a power cycle and had to be reflashed through the JTAG port to recover them.

I dumped the flash contents of these 3 devices:

* The application spaces look good, no overwrites or partial writes

* The DCT1 and DCT2 sections are mostly erased

Here is the first 128 bytes of DCT1, from one device

00 00 00 00 00 00 00 00 00 01 00 42 52 43 4D FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF 01 FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF 00 00 00 00 00 00 00 00 00 00 00 00 14 BE 68 00 00 01 00 00 00 00 00 00 FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

Here is the first 128 bytes of DCT2, from one device

00 00 00 00 00 00 00 00 01 01 00 42 52 43 4D FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF 01 FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF 00 00 00 00 00 00 00 00 00 00 00 00 14 BE 68 00 00 01 00 00 00 00 00 00 FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

* The DCT Save area is not erased

Here is the first 128 bytes of DCT Save area, from one device

40 00 00 50 1F 00 00 00 01 01 00 42 52 43 4D 02 00 00 00 44 C0 20 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 01 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 01 00 00 00 00 00 00 00 14 BE 68 00 00 01 00 00 00 00 00 00 02 00 00 00 00 C0 20 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

To me, it seems that the factory image was in progress of being extracted, the old DCT was pushed to the save area and then something happened while erasing or writing the DCT1/2 areas.

What should happen if the DCT is corrupt?

At this point, the boot process appears to have been corrupted.

I looked a little further into the DCT, at the ota2 section, around offset 7972

FF FF 02 01

Update count = 0xFFFF

Boot type = 0x02

Force Factory Reset = 0x01

Any ideas what happened? This does not seem completely fail safe.

Proc: CYW43907

SDK: 6.2.1

0 Likes
3 Replies
NiMc_1688136
Level 5
Level 5
10 sign-ins 50 questions asked 10 solutions authored

After a power cycle there was no serial output from the ota2 extraction app (enabled).

The bootloader does not have stdio enabled

The failsafe app did not print anything (enabled)

0 Likes
lock attach
Attachments are accessible only for community members.

DCT1 and DCT2 attached

0 Likes

On the device from earlier in the week, during the watchdog events on boot, there is garbgage data for the DHCP CLIENT hostname line, which i think is from the DCT. Could there have been either a DCT corruption with this device too, or the voltage was too low to read from flash?

"10/8/2019 1:25:02 PM",Starting WICED vWiced_006.002.001.0002

"10/8/2019 1:25:02 PM",Initialising LwIP v2.0.3

"10/8/2019 1:25:02 PM",Starting WICED vWiced_006.002.001.0002

"10/8/2019 1:25:02 PM",Initialising LwIP v2.0.3

"10/8/2019 1:25:02 PM",DHCP CLIENT hostname ÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿ

"10/8/2019 1:25:03 PM",Starting WICED vWiced_006.002.001.0002

"10/8/2019 1:25:03 PM",Initialising LwIP v2.0.3

"10/8/2019 1:25:03 PM",DHCP CLIENT hostname ÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿ

"10/8/2019 1:25:03 PM",Starting WICED vWiced_006.002.001.0002

"10/8/2019 1:25:03 PM",Initialising LwIP v2.0.3

"10/8/2019 1:25:03 PM",DHCP CLIENT hostname ÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿ

"10/8/2019 1:25:03 PM",Starting WICED vWiced_006.002.001.0002

"10/8/2019 1:25:03 PM",Initialising LwIP v2.0.3

"10/8/2019 1:25:03 PM",DHCP C

0 Likes