- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I am using the pioneer kit CY8CKIT_062 with WiFi-BT.
When I compile and flash the kit using WICED, I get the following error
Building apps lookup table
Downloading Bootloader ...
"**** OpenOCD failed - ensure you have installed the driver from the drivers directory, and that the debugger is not running **** In Linux this may be due to USB access permissions. In a virtual machine it may be due to USB passthrough settings. Check in the task list that another OpenOCD process is not running. Check that you have the correct target and JTAG device plugged in. ****"
Downloading DCT ...
"**** OpenOCD failed - ensure you have installed the driver from the drivers directory, and that the debugger is not running **** In Linux this may be due to USB access permissions. In a virtual machine it may be due to USB passthrough settings. Check in the task list that another OpenOCD process is not running. Check that you have the correct target and JTAG device plugged in. ****"
Downloading resources filesystem ... build/demo.aws.iot.pub_sub.publisher-CY8CKIT_062/filesystem.bin at sector 1 size 97...
tools/makefiles/wiced_apps.mk:334: recipe for target 'FILESYSTEM_IMAGE_DOWNLOAD' failed
- make.exe[1]: *** [FILESYSTEM_IMAGE_DOWNLOAD] Error 1
- make.exe[1]: *** Waiting for unfinished jobs....
Makefile:351: recipe for target 'main_app' failed
make: *** [main_app] Error 2
10:59:23 Build Finished (took 20s.89ms)
The content of the openOCD.log file is
Open On-Chip Debugger 0.10.0+dev-00227-g0d15c62 (2018-03-27-15:19)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
Info : auto-selecting first available session transport "swd". To override use 'transport select <transport>'.
adapter speed: 1000 kHz
cortex_m reset_config sysresetreq
cortex_m reset_config vectreset
post_init_psoc6_setup
Error: CMSIS-DAP: SWD not supported
I am using Programmer 3.28.4. A snapshot of what programmer shows is attached
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
The firmware version required for CMSIS-DAP is 1.10.
Info : CMSIS-DAP: FW Version = 1.10
It can be found from openocd_log.txt file in build folder.
Kindly update the DAPLink Firmware and to update the firmware, please refer the below KitProg3 user guide link :
https://www.cypress.com/file/452701/download
Thanks.