Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Wi-Fi Combo

ShAb_4059181
Level 2
Level 2

I am using the pioneer kit CY8CKIT_062 with WiFi-BT.

When I compile and flash the kit using WICED, I get the following error

Building apps lookup table

Downloading Bootloader ...

"**** OpenOCD failed - ensure you have installed the driver from the drivers directory, and that the debugger is not running **** In Linux this may be due to USB access permissions. In a virtual machine it may be due to USB passthrough settings. Check in the task list that another OpenOCD process is not running. Check that you have the correct target and JTAG device plugged in. ****"

Downloading DCT ...

"**** OpenOCD failed - ensure you have installed the driver from the drivers directory, and that the debugger is not running **** In Linux this may be due to USB access permissions. In a virtual machine it may be due to USB passthrough settings. Check in the task list that another OpenOCD process is not running. Check that you have the correct target and JTAG device plugged in. ****"

Downloading resources filesystem ... build/demo.aws.iot.pub_sub.publisher-CY8CKIT_062/filesystem.bin at sector 1  size 97...

tools/makefiles/wiced_apps.mk:334: recipe for target 'FILESYSTEM_IMAGE_DOWNLOAD' failed

  1. make.exe[1]: *** [FILESYSTEM_IMAGE_DOWNLOAD] Error 1
  2. make.exe[1]: *** Waiting for unfinished jobs....

Makefile:351: recipe for target 'main_app' failed

make: *** [main_app] Error 2

10:59:23 Build Finished (took 20s.89ms)

The content of the openOCD.log file is

Open On-Chip Debugger 0.10.0+dev-00227-g0d15c62 (2018-03-27-15:19)

Licensed under GNU GPL v2

For bug reports, read

       http://openocd.org/doc/doxygen/bugs.html

Info : auto-selecting first available session transport "swd". To override use 'transport select <transport>'.

adapter speed: 1000 kHz

cortex_m reset_config sysresetreq

cortex_m reset_config vectreset

post_init_psoc6_setup

Error: CMSIS-DAP: SWD not supported

I am using Programmer 3.28.4.  A snapshot of what programmer shows is attached


0 Likes
1 Solution
KotnaniK_71
Employee
50 likes received 25 likes received 10 likes received
Employee

Hi,

The firmware version required for CMSIS-DAP is 1.10.

Info : CMSIS-DAP: FW Version = 1.10

It can be found from openocd_log.txt file in build folder.

Kindly update the DAPLink Firmware and to update the firmware, please refer the below KitProg3 user guide link :

https://www.cypress.com/file/452701/download

Thanks.

View solution in original post

0 Likes
8 Replies
KotnaniK_71
Employee
50 likes received 25 likes received 10 likes received
Employee

Hi,

Could you please provide the screenshot of your device manager window?

0 Likes
KotnaniK_71
Employee
50 likes received 25 likes received 10 likes received
Employee

Hi,

Could you please try to change the mode of SW4 switch and update us.

0 Likes
ShAb_4059181
Level 2
Level 2

before pressing SW4, the state of the LEDs are as follows:

LED2 Blinking yellow

LED3 off

LED1 off

LED4 solid yellow

When I press SW4

LED2 Blinking Yellow

LED3 Solid Green

LED1 Solid Red

LED4 Off

WHen I compile and download, I get

Building apps lookup table

Downloading Bootloader ...

"**** OpenOCD failed - ensure you have installed the driver from the drivers directory, and that the debugger is not running **** In Linux this may be due to USB access permissions. In a virtual machine it may be due to USB passthrough settings. Check in the task list that another OpenOCD process is not running. Check that you have the correct target and JTAG device plugged in. ****"

Downloading DCT ...

"**** OpenOCD failed - ensure you have installed the driver from the drivers directory, and that the debugger is not running **** In Linux this may be due to USB access permissions. In a virtual machine it may be due to USB passthrough settings. Check in the task list that another OpenOCD process is not running. Check that you have the correct target and JTAG device plugged in. ****"

Downloading resources filesystem ... build/demo.aws.iot.pub_sub.publisher-CY8CKIT_062/filesystem.bin at sector 1  size 97...

tools/makefiles/wiced_apps.mk:334: recipe for target 'FILESYSTEM_IMAGE_DOWNLOAD' failed

make.exe[1]: *** [FILESYSTEM_IMAGE_DOWNLOAD] Error 1

make.exe[1]: *** Waiting for unfinished jobs....

Makefile:351: recipe for target 'main_app' failed

make: *** [main_app] Error 2

08:41:30 Build Finished (took 19s.35ms)

the content of the openocd_log.txt is

Open On-Chip Debugger 0.10.0+dev-00227-g0d15c62 (2018-03-27-15:19)

Licensed under GNU GPL v2

For bug reports, read

http://openocd.org/doc/doxygen/bugs.html

Info : auto-selecting first available session transport "swd". To override use 'transport select <transport>'.

adapter speed: 1000 kHz

cortex_m reset_config sysresetreq

cortex_m reset_config vectreset

post_init_psoc6_setup

Error: unable to find CMSIS-DAP device

Thank you for your help

0 Likes
KotnaniK_71
Employee
50 likes received 25 likes received 10 likes received
Employee

Hi,

The firmware version required for CMSIS-DAP is 1.10.

Info : CMSIS-DAP: FW Version = 1.10

It can be found from openocd_log.txt file in build folder.

Kindly update the DAPLink Firmware and to update the firmware, please refer the below KitProg3 user guide link :

https://www.cypress.com/file/452701/download

Thanks.

0 Likes
ShAb_4059181
Level 2
Level 2

I try to use the programmer to upgrade the firmware, but I remain on the same version of the firmware.

Would you kindly provide specific instructions.

Shukri

0 Likes
ShAb_4059181
Level 2
Level 2

I upgraded using the command below fw-loader.exe –update-kp3, but programmer wants me to revert. See programmer’s output below

C:\Users\sabdalla\ModusToolbox_1.1\tools\fw-loader-2.1\bin>fw-loader.exe --update-kp3

Cypress Firmware Updater, Version: 2.1.0.52

(C) Copyright 2018-2019 by Cypress Semiconductor

All Rights Reserved

Info: Start API initialization

Info: Connected - KitProg3 CMSIS-DAP HID-04170E6C03227400

Info: Hardware initialization complete (633 ms)

Device 'KitProg3 CMSIS-DAP HID-04170E6C03227400' opened successfully

Info: Kit FW is 'KitProg3' ver. 1.01 b158. Upgrade file is 'KitProg3' ver. 1.10 b2946. Upgrade file contains a Custom App.

Info: Disconnected - KitProg3 CMSIS-DAP HID-04170E6C03227400

Info: Connected - KitProg Bootloader-04170E6C03227400

Info: Bootloader Version: Major 1, Minor 1, Build 40

Info: FW Upgrade to version: 1.10 b2946. Upgrade of Custom App

Info: Bootloading of Custom App...

Info: Verifying of Custom App...

Info: Bootloading of KitProg FW...

Info: Verifying of KitProg FW...

Info: Upgrade completed

Info: Disconnected - KitProg Bootloader-04170E6C03227400

Info: Connected - KitProg3 CMSIS-DAP HID-04170E6C03227400

FW update completed successfully

0 Likes
KotnaniK_71
Employee
50 likes received 25 likes received 10 likes received
Employee

Hi,

Can you please try now programming through Wiced by using SW4 switch in DAP link mode and let us know if downloading the resource file system is happening or not.

Thanks.

0 Likes