Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Wi-Fi Combo Forum Discussions

cohuc_3807591
Level 3
Level 3
5 likes given First like given

SDK being used - 6.0

So I'm trying to use OTA2 on the quicksilver arrow platform (cyw43907 based). I added the platform files to WICED, added the platform as valid for the ota2 bootloader and failsafe, and built the OTA2 example code and it works flawlessly. However when I try to download the ota2 image file (snip.scan, built with make target snip.scan-QuicksilverEval ota2_image) the ota2 code reports that the platform in the header isn't correct. heres the log output:

0273 00:10:45.458 wiced_ota2_image_validate() OTA Image Platform type fail. CYW943907AEVAL1F.B1 != QuicksilverE             val

0274 00:10:45.467 wiced_ota2_write() wiced_ota2_update_staged_header() OTA image not supported!

0276 00:10:45.578 OTA header Information: OTA Image Header after Updating OTAImage header:

0277 00:10:45.585        ota_version: 1

0278 00:10:45.589     software_major: 0

0279 00:10:45.592     software_minor: 0

0280 00:10:45.596           platform: CYW943907AEVAL1F.B1

0281 00:10:45.601             status: 0 (invalid)

0282 00:10:45.606     bytes_received: 1215

0283 00:10:45.609         header_crc: 0x1acf1f42

0284 00:10:45.614       magic_string: OTAimage

0285 00:10:45.618          sign_type: 0

0286 00:10:45.622   secure_signature: TODO

0287 00:10:45.626         image_size: 937984

0288 00:10:45.630    component_count: 5

0289 00:10:45.633  data start offset: 4096

0290 00:10:45.637 ota2_get_OTA() FAILED 0 < 937984!

0291 00:10:45.642

ota2_get_OTA_file() Exiting 4

What do I need to change (not including updating the WICED version) to ensure that the ota2 header is written with the proper platform?

0 Likes
1 Solution

Can you please confirm the platform name in generated ota2_image file? Open the OTA2_image_file.bin file with any hex editor:

pastedImage_0.png

View solution in original post

0 Likes
4 Replies
PriyaM_16
Moderator
Moderator
Moderator
25 solutions authored 10 solutions authored 5 solutions authored

Use the same platfrom name for both the platforms. Are you using different platform file while creating the target?

0 Likes

The platform name is the same for both platforms:

snip.ota2_extract-QuicksilverEval

snip.ota2_example-QuicksilverEval ota2_image download_apps download run

snip.scan-QuicksilverEval ota2_image

0 Likes

Can you please confirm the platform name in generated ota2_image file? Open the OTA2_image_file.bin file with any hex editor:

pastedImage_0.png

0 Likes

Hello,

Please let me know if you were able to do an OTA update.

0 Likes