- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi vik86 and peter_fenn
Per this thread: OTA upgrade stuck at Restarting.. on the terminal window
I am working on avnet iot kit and i also facing the same issue of getting stuck at the restart point. Now if I do a hard reboot the device doesn't show any logs at all. I need to flash a new application if I need to get it work again. Can anyone help on this one
Thanks in advance for your help
Solved! Go to Solution.
- Labels:
-
AWS
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Do you had patch your 3.5.2 SDK according Possible 3.5.2 bug in wiced_framework_set_boot() ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
could you share your make build target you are using to download the application ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I am using the command snip.ota_fr-BCM94343W_AVN download_apps run
I am attaching the logs I am getting also with this
Starting WICED v3.5.2
Platform STMF405 initialised
Started ThreadX v5.6
Initialising NetX_Duo v5.7_sp2
Creating Packet pools
WWD SDIO interface initialised
WLAN MAC Address : 6C:0B:84:D1:32:43
WLAN Firmware : wl0: Nov 25 2015 12:57:14 version 7.45.45.1 (r602358) FWID 01-1920c040
Mutex Init Done
Time for an upgrade. OTA upgrade starting ...
IPv4 network ready IP: 192.168.10.1
Setting IPv6 link-local address
IPv6 network ready IP: FE80:0000:0000:0000:6E0B:84FF:FED1:3243
**************************************
Your SSID : Molekule Device
Your PASSPHRASE : molekule123
Your web bowzer : 192.168.10.1
**************************************
Going to create the Device_Manager thread
Writing chunk 1 of size 1024 from offset 0
Writing chunk 2 of size 1024 from offset 1024
Writing chunk 3 of size 1024 from offset 2048
Writing chunk 4 of size 1024 from offset 3072
Writing chunk 5 of size 1024 from offset 4096
Writing chunk 6 of size 1024 from offset 5120
Writing chunk 7 of size 1024 from offset 6144
Writing chunk 8 of size 1024 from offset 7168
Writing chunk 9 of size 1024 from offset 8192
Writing chunk 10 of size 1024 from offset 9216
Writing chunk 11 of size 1024 from offset 10240
Writing chunk 12 of size 1024 from offset 11264
Writing chunk 13 of size 1024 from offset 12288
Writing chunk 14 of size 1024 from offset 13312
Writing chunk 15 of size 1024 from offset 14336
Writing chunk 16 of size 1024 from offset 15360
Writing chunk 17 of size 1024 from offset 16384
Writing chunk 18 of size 1024 from offset 17408
Writing chunk 19 of size 1024 from offset 18432
Writing chunk 20 of size 1024 from offset 19456
Writing chunk 21 of size 1024 from offset 20480
Writing chunk 22 of size 1024 from offset 21504
Writing chunk 23 of size 1024 from offset 22528
Writing chunk 24 of size 1024 from offset 23552
Writing chunk 25 of size 1024 from offset 24576
Writing chunk 26 of size 1024 from offset 25600
Writing chunk 27 of size 1024 from offset 26624
Writing chunk 28 of size 1024 from offset 27648
Writing chunk 29 of size 1024 from offset 28672
Writing chunk 30 of size 1024 from offset 29696
Writing chunk 31 of size 1024 from offset 30720
Writing chunk 32 of size 1024 from offset 31744
Writing chunk 33 of size 1024 from offset 32768
Writing chunk 34 of size 1024 from offset 33792
Writing chunk 35 of size 1024 from offset 34816
Writing chunk 36 of size 1024 from offset 35840
Writing chunk 37 of size 1024 from offset 36864
Writing chunk 38 of size 1024 from offset 37888
Writing chunk 39 of size 1024 from offset 38912
Writing chunk 40 of size 1024 from offset 39936
Writing chunk 41 of size 1024 from offset 40960
Writing chunk 42 of size 1024 from offset 41984
Writing chunk 43 of size 1024 from offset 43008
Writing chunk 44 of size 1024 from offset 44032
Writing chunk 45 of size 1024 from offset 45056
Writing chunk 46 of size 1024 from offset 46080
Writing chunk 47 of size 1024 from offset 47104
Writing chunk 48 of size 1024 from offset 48128
Writing chunk 49 of size 1024 from offset 49152
Writing chunk 50 of size 1024 from offset 50176
Writing chunk 51 of size 1024 from offset 51200
Writing chunk 52 of size 1024 from offset 52224
Writing chunk 53 of size 1024 from offset 53248
Writing chunk 54 of size 1024 from offset 54272
Writing chunk 55 of size 1024 from offset 55296
Writing chunk 56 of size 1024 from offset 56320
Writing chunk 57 of size 1024 from offset 57344
Writing chunk 58 of size 1024 from offset 58368
Writing chunk 59 of size 1024 from offset 59392
Writing chunk 60 of size 1024 from offset 60416
Writing chunk 61 of size 1024 from offset 61440
Writing chunk 62 of size 1024 from offset 62464
Writing chunk 63 of size 1024 from offset 63488
Writing chunk 64 of size 1024 from offset 64512
Writing chunk 65 of size 1024 from offset 65536
Writing chunk 66 of size 1024 from offset 66560
Writing chunk 67 of size 520 from offset 67584
Uploaded file size = 68104
Restarting..
After this even if you wait for 5-10 minutes also nothing is coming
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Which application you download via ota_fr, why the size only 66KB ?
Does the application work if down directly ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Its just a hello world printf program which when run directly its working. Even I tried a sample Timer program with that one also the same behavior is seen.
Hi Vik,
As you said I tried with the snip.ota_fr-BCM94343W_AVN download download_apps run but still the same behavior is seen
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
snip.ota_fr-BCM94343W_AVN download download_apps run
Can you modify it to the above build string and try. You are missing download. download_apps downloads it to the external serial flash alone.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Also I am working on a prototype board which uses the BCM4343WA1 module and the MCU is STMF405. We have an external flash also. So how can I flash those information about the app_look up table,etc to the external flash which is required for the OTA upgrade I believe.
When I debugged I found that in the wiced_apps_write some information is being taken from the external flash like where to keep the new image on the external flash etc. I am using dfu programmer or STLink utility to flash my image to the board, can I some how add these also as a part of my make target
example build make target will be like
snip.ota_fr-STMF405-debug
which will create your bootloader.bin, DCT.bin and app.bin which I will flash at particular locations
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Any updates
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Do you had patch your 3.5.2 SDK according Possible 3.5.2 bug in wiced_framework_set_boot() ?