- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Support,
I am evaluating the cypress CYW943907AEVAL1F board. Mostly I want to go for the wireless power save mode. I am following the document given at the link: Low Power Current Measurements Using CYW943907AEVAL1F .
As mentioned in the document I am using an example 43xxx_Wi-Fi/apps/test/powersave/powersave.c and enabling the macro POWERSAVE_STANDALONE_TEST_DEEPSLEEP_ASSOC. As mentioned in the document I should get the current around ~1-2 mA. But I am getting around ~16 mA at least as the lowest. Please find the attached snap-shot FYR. I am attahcing the application file also whatever I am using. I also tried to reduce the becon size by disabling WMM, WPS, enablig only 11b as mentioned in one of the document by cyoress.
Can you please tell me whether I am missing something in the configuration? Do I need to do any other board changes to achieve low numbers?
Thanks
Akash
Solved! Go to Solution.
- Labels:
-
ispn:38946:1:0
-
l1:314:1:0
-
WirelessMCU
- Tags:
- power_number
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
FYI,
It looks like the same issue reported below:
https://community.cypress.com/message/160646#160646
vikr mentioned that "There is an issue with 6.2 SDK, we are working on the fix".
However, there is no follow up so no fix available yet.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
FYI,
It looks like the same issue reported below:
https://community.cypress.com/message/160646#160646
vikr mentioned that "There is an issue with 6.2 SDK, we are working on the fix".
However, there is no follow up so no fix available yet.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Okay, Thanks for the reply.
Then for the stable number which SDK version do you suggest, I should use ?
And moreover, I feel this is not the same issue with the (CYW43907) powersave test app - verify that it is working as intended . As mentioned in that discussion they are at least getting ~300 uA for sleep interval. I am not getting the same number in sleep also.
But as you suggested there is some issue with the latest SDK so can I know when will it get fixed. Or it would be great if you can suggest the preferable SDK version.
Thanks
Akash
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
You can roll back to WS 6.0.1 for the moment which can be downloaded from WICED-Studio 6.0.1 Installer (Windows) . We will update the thread once the fix is integrated with the future release.