Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Hi All

        Not able to get SNTP Response, It giving up after trying two times with attached logs.

/* Bringup the network interface */

    wiced_network_up( WICED_STA_INTERFACE,WICED_USE_EXTERNAL_DHCP_SERVER, NULL );

logs:

Starting WICED v3.1.2

Platform BCM9WCDPLUS114 initialised

Started ThreadX v5.6

Initialising NetX_Duo v5.7_sp1

Creating Packet pools

WWD SDIO interface initialised

WLAN MAC Address : FC:4D:D4:FF:C3:7A

WLAN Firmware    : wl0: Nov  7 2014 16:03:45 version 5.90.230.12 FWID 01-4b73cbac

Starting WICED Bluetooth

Bluetooth MAC Address : FC:4D:D4:ED:0D:30

Bluetooth Firmware    : BCM20702B0_002.001.014.0487.0000_Generic_UART_Class1_20MHz.hcd

Initialising WICED SmartBridge ...

Joining : SMART

Successfully joined : SMART

Obtaining IPv4 address via DHCP

Setting IPv6 link-local address

IPv4 network ready IP: 10.100.10.64

Getting NTP time...

failed, trying again...

failed, trying again...

failed, trying again...

Give up getting NTP time

0 Likes
3 Replies
VikramR_26
Employee
Employee
25 sign-ins 10 sign-ins 10 comments on KBA

Just to confirm does your SMART access point connected to internet ?

0 Likes
Anonymous
Not applicable

yes its connected !

0 Likes

1. Check your AP/Router could access internet well!

2. Check your DHCP client get the correct IP address/netmask/gateway and DNS from DHCP server!

3. Check your hostname lookup get response from DNS server when call SNTP!

4. Does your gateway/firewall allow SNTP protocol pass through  ?

0 Likes