Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Wi-Fi Combo Forum Discussions

Anonymous
Not applicable

I want to use bt_smartbridge_mfg_test coming with WICED-SDK-3.0.1. I found a brief description with .c file as blow, but when I google "bluetool", it doesn't turn up meaningful links. what is bluetool? How to get it?

Thanks,

Xinsi

* Copyright 2014, Broadcom Corporation
* All Rights Reserved.
*
* This is UNPUBLISHED PROPRIETARY SOURCE CODE of Broadcom Corporation;
* the contents of this file may not be disclosed to third parties, copied
* or duplicated in any form, in whole or in part, without the prior
* written permission of Broadcom Corporation.
*/

/** @file
*
* Bluetooth SmartBridge Manufacturing Test Application
*
* This application enables users to access the local Bluetooth
* device using a PC manufacturing test application such as BlueTool.
*
* Application Instructions
*   1. Connect a PC terminal to the serial port of the WICED Eval board,
*      then build and download the application as described in the WICED
*      Quick Start Guide
*   2. Run BlueTool on your computer
*   3. Select Transport | HCI Control | UART
*   4. Enter the corresponding COM port and set the baud rate to 115200.
*      Ensure that 'CTS flow control and 'SLIP/Three-wire' are unticked and then
*      click 'OK'. The HCI command window appears
*   5. Select View | Log Window. The log window appears
*   6. Double-click on your desired HCI command to send
*/

0 Likes
1 Reply
MichaelF_56
Moderator
Moderator 250 sign-ins 25 comments on blog 10 comments on blog
Moderator

Unfortunatley, Bluetool is an internal test tool and not available here on the community.

0 Likes