- USB-JTAG functionality
- USB-UART functionality
# udev rules file for WICED USB JTAG interface, to allow use by non super-usersSUBSYSTEM=="usb", ATTR{idVendor}=="0a5c", ATTR{idProduct}=="43fa", GROUP="hwlab", MODE="0666"To load the USB-UART driver , issue the following command on the command line (this could also be put into a Linux startup routine)The Serial port will be available on /dev/ttyUSB1 (or possibly a different ttyUSBx interface if other ttyUSB devices are already present)
sudo modprobe ftdi_sio vendor=0x0a5c product=0x43fa
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Nice, it works for me (Ubuntu 13.10).
I've added this line in /etc/modules for automatic startup:
ftdi_sio vendor=0x0a5c product=0x43fa
Tested with minicom (apt-get install minicom). The current user must be in the 'dialout' group:
minicom -D /dev/ttyUSB1
The default settings are correct (115200N81), press reset on the evaluation board you'll see the Wiced startup messages.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
For kernels >= 3.12 the product/vendor arguments to the module won't work.
Do this instead:
echo 0a5c 43fa > /sys/bus/usb-serial/drivers/ftdi_sio/new_id
That works for me on Kubuntu 14.04
Or for something more permanent:
cat /etc/udev/rules.d/90-wiced-driver.rules
ACTION=="add", SUBSYSTEMS=="usb", ATTRS{idVendor}=="0a5c", ATTRS{idProduct}=="43fa", GROUP="users", MODE="0666", RUN+="/lib/udev/wiced"
cat /lib/udev/wiced
#!/bin/sh
/sbin/modprobe ftdi_sio & echo 0a5c 43fa > /sys/bus/usb-serial/drivers/ftdi_sio/new_id
Jason H.