HI I purchased one EVK from Laird
455-00030 Laird - Wireless & Thermal Systems | RF/IF and RFID | DigiKey
I tried a few sample and attached to terminal
Both platform does not log anything after the joining log entry.
Am I missing custom platform files from Laird ?
CYW94343WWCD1_EVB
Description : Cypress BCM94343WWCD1 mounted on a Cypress CYW9WCD9EVAL evaluation board
BCM94343WWCD2
Description : Cypress BCM94343WWCD2 mounted on a Cypress BCM9WCD9EVAL1 evaluation board
Starting WICED Wiced_006.004.000.0061
Platform CYW94343WWCD1_EVB initialised
Started ThreadX v5.8
WICED_core Initialized
Initialising NetX_Duo v5.10_sp3
Creating Packet pools
Connect to the network
Joining : SSIDSAMPLE-2.4
Starting WICED Wiced_006.004.000.0061
Platform BCM94343WWCD2 initialised
Started ThreadX v5.8
WICED_core Initialized
Initialising NetX_Duo v5.10_sp3
Creating Packet pools
Connect to the network
Joining : SSIDSAMPLE-2.4
Solved! Go to Solution.
The BLE Wi-Fi introducer example should work with your module. Please add the platform name under VALID_PLATFORMS in ble_wifi_introducer.mk.
Never mind I didn't deploy the LAIRD_EWB platform files.
Can the BLE WIFI Introducer APP work with the Cypress WIFI used by Sterling module
Laird is providing an app called the EWB Mobile APP but it doesn't look like it comes with source code
To configure and connect the Sterling-EWB for your local Wi-Fi network, Laird provides the EWB mobile app. This application walks you through the following: ▪ Creating an account ▪ Scanning and connecting to your Sterling-EWB over BLE ▪ Scanning for, selecting, and providing the passphrase for the Wi-Fi network to your Sterling-EWB ▪ Provisioning the client for use on the demo
The BLE Wi-Fi introducer example should work with your module. Please add the platform name under VALID_PLATFORMS in ble_wifi_introducer.mk.