Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
shra_2185826
Level 2
Level 2
First like received

Hi

I am writing steps which I took to try the snip for OTA.

1. Compiled ota_fr snip with command for WICED dev board BCM943362WCD4_EVB.

make snip.ota_fr-BCM943362WCD4-FreeRTOS-LwIP-SDIO download download_apps run

Build and app donwload finishes successfully.

2. Built snip scan with

make snip.scan-BCM943362WCD4-FreeRTOS-LwIP-SDIO

3. Connected with the AP mode published by WICED .

4. In Browser opened http://192.168.10.1, OTA web page appears.

5. browse and select snip.scan-BCM943362WCD4-FreeRTOS-LwIP-SDIO.stripped.elf for OTA download.

6. Starts download. Shows transfer progress bar running.when it reaches 100% WICED device reboots with OTA snip itself while my expectation was that it will reboot with scan snip.

7. While debugging the same observed that in function process_upgrade_chunk API named wiced_framework_set_boot ( DCT_APP0_INDEX, PLATFORM_DEFAULT_LOAD ); returns failure.

I could not able to put debug print in that API as than it started to give compilation error of some BTLDR memory exceed.

So my suspicion is that while I have been able to download the file alright in section of memory for downloaded code.

I have not been able to flag it to bootloader to pick that code from that section into main app code memory section.

Can anyone verify my steps followed and point me to if there is any mistake ?

If it's known issue than is there any solution/workaround available to try out ?

Cheers,

Shishir

0 Likes
1 Solution

This workaround suggested by garywiz worked for me

It's not authorized by WICED team though.

You may use it until WICED team comes up with the fix.

Shishir

View solution in original post

0 Likes
7 Replies
VikramR_26
Employee
Employee
25 sign-ins 10 sign-ins 10 comments on KBA

There has been issues with OTA, since the DCT structure has been changed.

0 Likes

Hi vik86

Since you pointed out there are some known issues with OTA on SDK-3.5.2,

what's your suggestion for the users?

Would you provide the fix or otherwise users have no choice but to use

older SDK.

0 Likes

Hi Axel,

definitely we are working on the fix , we will provide the fix soon. you would not be stuck to a version of SDK for OTA . Main reason is change in the DCT structure and bootloader settings accordingly.

thnx

vik86

0 Likes

This workaround suggested by garywiz worked for me

It's not authorized by WICED team though.

You may use it until WICED team comes up with the fix.

Shishir

0 Likes

Possible 3.5.2 bug in wiced_framework_set_boot()

Forgot to put the above link in last message

0 Likes
Anonymous
Not applicable

skrawat

I also encountered the same issue reported here for the target SN8205x. After the rebooting WICED device reboots with OTA snip itself while my expectation was that it will reboot with scan snip. You suggested this workaround of wiced_framework_set_boot() but which file i need to put this function.

Thanks

0 Likes
Anonymous
Not applicable

Wiced_waf_common.c

0 Likes