Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

RaD_4001476
Level 1
Level 1
First like given

Hi,

I am facing below issue in connecting a JLink with ISM43362. I am trying to debug my application using Jlink.

I am using WICED SDK 6.4. Any help or pointers in resolving this will be helpful.

Below is the error:

SEGGER J-Link GDB Server V6.62 Command Line Version

JLinkARM.dll V6.62 (DLL compiled Jan 24 2020 16:32:09)

Command line: -if jtag -device CYW43362 -endian little -speed 1000 -port 2331 -swoport 2332 -telnetport 2333 -vd -ir -localhostonly 1 -singlerun -strict -timeout 0 -nogui

-----GDB Server start settings-----

GDBInit file:                  none

GDB Server Listening port:     2331

SWO raw output listening port: 2332

Terminal I/O port:             2333

Accept remote connection:      localhost only

Generate logfile:              off

Verify download:               on

Init regs on start:            on

Silent mode:                   off

Single run mode:               on

Target connection timeout:     0 ms

------J-Link related settings------

J-Link Host interface:         USB

J-Link script:                 none

J-Link settings file:          none

------Target related settings------

Target device:                 CYW43362

Target interface:              JTAG

Target interface speed:        1000kHz

Target endian:                 little

Connecting to J-Link...

J-Link is connected.

Failed to set device (CYW43362). Unknown device selected?ERROR : Failed to set device.

GDBServer will be closed...

Shutting down...

Strict limitation error. Please check for correct device name and settings.

Thanks,

Raghu

1 Solution
GauravS_31
Moderator
Moderator
Moderator
250 solutions authored 250 sign-ins First comment on KBA

It appears that the VID, PID has not been set correctly. Please contact your module partner to get the JTAG settings reviewed.

View solution in original post

1 Reply
GauravS_31
Moderator
Moderator
Moderator
250 solutions authored 250 sign-ins First comment on KBA

It appears that the VID, PID has not been set correctly. Please contact your module partner to get the JTAG settings reviewed.