cancel
Showing results for 
Search instead for 
Did you mean: 

Wi-Fi Combo

Anonymous
Not applicable
[WICED-SDK-2.2.1]

I need to know info about the AP my device is connected to, how do I get this?
0 Likes
3 Replies
Anonymous
Not applicable
An API to get this info will be added in the next SDK release, until then,

please read the information & patch in the source code provided in the attached file.
0 Likes
Anonymous
Not applicable
Thanks for the code snippets to retreive the AP details of the connected AP. However, there seems to be a small bug in returned results.

Ive updated this code to translate the bss_info_t to ap_info_t just as in the scan_result_handler.

But when I do this in the wiced_wifi_get_ap_info() function I get the wrong security type.

Ive connected to a WPA2_AES network, but the functions returns that it is WEP_PSK.

The scan results, using the same translation code, are OK.
0 Likes
Anonymous
Not applicable
Hmm.. Ill need to investigate this further.

The scan result handler determines the security setting by parsing the IEs in the probe responses however I am not sure if all that information is kept in the same format in the wl_bss_info_t structure.

Ill look into it and get back to you.
0 Likes